Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • All About Jitter

    01/26/2017

    Though a detailed explanation of jitter can be highly complex mathematically, simply put, jitter is the deviation of a signal from its ideal periodic behavior in terms of frequency, signal amplitude, or phase. There are many contributors to jitter in a signal, from the source itself to outside interferers. Additionally, jitter can be described similarly ..

    Read Full Article

    5G Requirements

    01/19/2017

    Though no single 5G requirement is yet set in stone, there has been some consensus from various industrial partnerships, standards bodies, and regulatory agencies on a vision for 5G. Some aspects of this vision are debated as to when they may be realized, but a common timeframe is to have a full 5G definition with ..

    Read Full Article

    Fixed Attenuators 101

    01/12/2017

    RF attenuators are used to reduce the level of a signal. Some reasons why you might want to reduce the signal level would be to protect a circuit stage from receiving a signal that is too high or in applications where a signal level needs to be controlled. Attenuators typically consist of a resistive network ..

    Read Full Article

    Tips for Assembling, Troubleshooting and Handling Waveguides

    01/05/2017

    Though waveguide components and interconnects tend to be formed of relatively sturdy metals, some aluminum and copper waveguides, for higher frequency and aerospace applications, can easily be dinged and dented. Sometimes these dings and dents are a useful tuning technique; generally, they could dramatically change the performance of a waveguide or waveguide component. Ensuring that ..

    Read Full Article

    2016 IME/China Expo, Wrap Up

    11/03/2016

    We just wrapped up another successful year at IME/China in Shanghai. The China International Conference & Exhibition on Microwave and Antenna (IME/China) is the largest and most influential RF, microwave and antenna exhibition in China. It is “the” place to be for RF design engineers, technical managers and purchasing executives in China and from abroad. ..

    Read Full Article

    New Low Profile, Right Angle Test Cable Line Up to 27 GHz

    05/24/2016

    New SMA, Type N and TNC Test Cable Boast 1.25:1 Typical VSWR and 69.5% Phase Velocity We just launched a new family of right angle test cable with low profile design. These 16 unique test cable assemblies cover a frequency range from DC to 27 GHz for the SMA versions and DC to 18 GHz ..

    Read Full Article

    60 GHz Development System Kit Offers a Quick Out-of-the-Box Experience for Evaluating High Bandwidth Data Rates in the Unlicensed ISM Frequency Spectrum

    05/20/2016

    60 GHz Product Development System and Experimentation Kit for High Bandwidth Modulation Covering 57 to 64 GHz Made Easy The new 60 GHz development system kit, now with even lower phase noise,  offers designers the ability to perform millimeter wave product development and conduct RF experimentation. The developer kit for 60 GHz provides single and ..

    Read Full Article

    IMS 2016 IEEE MTT-S San Francisco, CA Pasternack Drone Contest

    05/17/2016

    We will be exhibiting at the IMS 2016 conference, convention and exposition which is now called the International Microwave Symposium 2016, formerly called MTT-S or the Microwave Theory and Techniques Society trade show, being held in San Francisco, CA for 2016. The IMS 2016 General Chair says “IMS2016, organized by the IEEE Microwave Theory and ..

    Read Full Article

    IEEE / MTT-S / International Microwave Symposium / IMS 2016

    05/09/2016

      Again this year we will be exhibiting at the IEEE conference, convention and exposition called the International Microwave Symposium / IMS, formerly called MTT-S or the Microwave Theory and Techniques Society trade show, which is held in San Francisco, CA for IMS 2016. According to the IEEE conference website previously, “the IEEE MTTS International ..

    Read Full Article

    PIN Diode Switch RF Product Line Now Largest Same Day Ship Selection

    04/28/2016

    Pasternack PIN Diode Switch Expanded to the Largest In-Stock, Same-Day Ship Inventory We greatly expanded our PIN diode switch products over the past several months to become THE source for your needs. Pasternack can now claim the largest selection of connectorized PIN diode switches in-stock for same day shipping. Our portfolio of in-stock solid state ..

    Read Full Article
    Jump to of 37
    Live help