Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • RF Amplifier Packaging and Thermal Dynamics

    04/06/2017

    Packaging dimensions, weight, pinouts and material construction are critical features of any RF amplifier. These factors heavily weigh into the cost and feasibility of using a particular amplifier in a given design. Regardless of electrical and RF performance, if an amplifier can’t fit into the required footprint, the device won’t be serviceable for that application. ..

    Read Full Article

    Cheap Waveguides can Ruin your Day

    03/30/2017

    Though there are many reputable and high quality waveguide vendors, some vendors, specifically offshore vendors, may use machining techniques that reduce time and cost of manufacture. These short-cuts could have dramatic impact on a waveguide component and system performance. Any misalignments or machined geometries beyond specified levels can reduce the VSWR performance of a waveguide, ..

    Read Full Article

    Practical Mixers 101

    03/23/2017

    Introduction to Mixers A microwave frequency mixer is a 3-port electronic circuit that combines two or more signals into one or two composite output signals, and are categorized as switching mixers or nonlinear mixers– although many mixers are configured with both. Using diodes, the mixer is passive and has a conversion loss. Using active devices, ..

    Read Full Article

    RF and Microwave Attenuator Fundamentals

    03/16/2017

    RF attenuators are fundamental components of RF and Microwave circuits and systems. Often found in virtually every RF application, attenuators play a vital role in receivers, transmitters, test and measurement systems etc. The main purpose of attenuators is to reduce the signal strength, such as prior to the signal reaching a sensitive circuit element. Attenuators ..

    Read Full Article

    RF Amplifier Power and Gain Considerations

    03/09/2017

    The input and output power characteristics of an RF amplifier are dominant characteristics, as increasing signal strength is the primary purpose of an amplifier. An RF amplifier will be specified with a maximum and nominal range for input and output power based on certain conditions. These specifications will further extend to a maximum and nominal ..

    Read Full Article

    RF Filter Overview – Types & Topologies

    03/02/2017

    RF filters are some of the most important components in receivers. The main functions of the filters are to reject undesirable signals outside the filter pass band and to separate signals according to their frequency. RF filters modify the amplitudes and phases of sinusoidal waveforms that pass through them or, more simply, RF filters remove unwanted ..

    Read Full Article

    Why Quality is Imperative for High Frequency Waveguides

    02/23/2017

    The quality of the construction and materials used can have a large impact on the performance of a waveguide system, especially in microwave frequencies and high power applications. This can become difficult to manufacture and evaluate, as the waveguide tolerances are extremely small at microwave and millimeter-wave frequencies. For instance, with millimeter-wave components and interconnects, ..

    Read Full Article

    Anatomy of a Coax Cable –and how they Work

    02/16/2017

    Coaxial cables are commonly known for being a broadband, relatively low-loss and high isolation transmission line technology. A coaxial cable is comprised of two concentric conductive cylinders separated by a dielectric spacer. The capacitance and inductance distributed along the coaxial line creates distributed impedance throughout the structure, known as characteristic impedance. The distributed resistive losses ..

    Read Full Article

    Antenna Gain and Directivity – The Basics

    02/09/2017

    What is antenna gain and directivity? Antennas, in essence, channel electrical power into electromagnetic signals. The shape, size, and connectorization all affect the antenna radiation pattern. Two key parameters in assessing the performance of an antenna are directivity and gain―directivity is a measurement of the concentration radiation in a direction while gain represents the power ..

    Read Full Article

    Directional Coupler and Power Divider/Combiner Overview

    02/02/2017

    Directional couplers are four port passive devices that employ an input port, output port, a port for the coupled signal and a port that is terminated internally. Directional couplers are used to couple a specific proportion of the power traveling in one transmission line out through another connection or port. Directional couplers are used in ..

    Read Full Article
    Jump to of 37
    Live help