Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • A Brief Introduction to the Types of RF Phase Shifters

    06/15/2017

    Phase Shifters are a critical component in many RF and Microwave systems. A phase shift module is a microwave network module which provides a controllable phase shift of the RF signal and are used in phased arrays. Phase shifters are used to change the transmission phase angle of a two-port network. Applications include controlling the ..

    Read Full Article

    Adapter and Terminator Considerations

    06/08/2017

    As every adapter and termination can introduce unwanted insertion loss and reflections. Carefully choosing the right component can prevent unwanted signal degradation and potential damage to sensitive electronics. Adapters and terminations come in many forms, generally coaxial or waveguide for high power applications. Additionally, adapters can be more complex as the sizes and types of ..

    Read Full Article

    RF Attenuator Applications

    06/01/2017

    Attenuators are an intrinsic part of many electrical designs, due to their utility in controlling amplitude and ability to improve the voltage standing wave ratio (VSWR) of a poorly matched load. Some applications include test set ups that leverage fixed attenuators as protection before test equipment to stay within the dynamic range of the equipment. ..

    Read Full Article

    Phase Noise and Additive Phase Noise Limit Radar and Communications System Performance

    05/25/2017

    Phase noise and its time-domain counterpart, jitter have been studied in radar and communications systems since the phenomenon was first observed. Though always a concern, recent advances in high-speed digital modulation schemes and advanced radar, which also used complex digital modulation techniques for pulse compression, have led to radar and communication systems being more susceptible ..

    Read Full Article

    The Difference between MIL-STD, MIL-HDBK, MIL-DTL, MIL-PRF and MIL-SPEC

    05/18/2017

    The US defense standards, commonly referred to as MilSpec, are developed by the US DoD for the purpose of enhancing interoperability among critical defense systems. The goal of the standards is to provide precise descriptions on the procedures and practices for the design, manufacturing, and deployment of military devices and equipment. Ultimately, the standards aim ..

    Read Full Article

    Waveguides Inside Out

    05/11/2017

    Following from the name, a waveguide is a hollow conductive structure that guides an EM wave along a path. The conductive inner walls of the waveguide bounce EM energy along the path with low-loss and close to light speed. Waveguides are commonly cylindrical, elliptical, or rectangular. In a rectangular waveguide, transverse electric (TE), or H-wave, ..

    Read Full Article

    When and Where You Need RF Limiters and Detectors

    05/04/2017

    RF limiters and detectors are used widely throughout the RF and microwave industry in a wealth of circuit applications. For example, radar transceivers, telecommunication radios, test and measurement equipment, and other circuits rely on RF limiters for receiver protection, as well as the protection of critical circuit components that may experience high-peak voltage and current ..

    Read Full Article

    What is Passive Intermodulation (PIM) Distortion, and how can it be Mitigated?

    04/27/2017

    Passive intermodulation (PIM) distortion is a wireless communication system degrading phenomenon that has been a concern for cellular telecommunications, satellite communications, and wireless network development. PIM is such a concern in cellular/wireless communications that there are entire distinct Low PIM Components and Cable Assemblies product lines designed to aid in preventing or mitigating PIM distortion. ..

    Read Full Article

    What you need to know about Reverse Polarized Connectors

    04/20/2017

    A reverse polarized coax connector is a variation of a standard polarity connector in which the gender of the interface has been reversed. The term “reverse polarity” refers not to the signal polarity of the connector itself but to the gender of the center contact pin. A reverse polarized connector will have the same external ..

    Read Full Article

    What do RoHS, REACH, and WEEE Mean for RF/Microwave Components, Manufacturers and Assemblers?

    04/13/2017

    RoHS, also known as Lead-Free, stands for Restriction of Hazardous Substances. RoHS originated in the European Union and restricts the use of six hazardous materials found in electrical and electronic products. All applicable products in the EU market after July 1, 2006 must pass RoHS compliance. The substances banned under RoHS are lead (Pb), mercury ..

    Read Full Article
    Jump to of 37
    Live help