Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • What is a Waveguide Magic Tee?

    01/19/2023

    A Waveguide Magic Tee is a 180-degree hybrid power divider with 4 ports made from a single waveguide structure. The Magic Tee has been around for over 70 years and was a product of development during World-War II. The structure of a Magic Tee is a combination of an E-plane waveguide arm meeting a H-plane ..

    Read Full Article

    SMA Connector Overview

    12/29/2022

    SMA Coaxial Connectors, or just SMAs, are one of the most common coaxial connector types used throughout the RF, microwave, and even millimeter-wave (mmW) industries. SMA stands for subminiature version A and was developed in the 1960s. The interface dimensions and other aspects of the SMA connector are detailed in MIL-STD-348 and was originally designed ..

    Read Full Article

    Coaxial Cable Assemblies for Rugged Outdoor Applications

    12/15/2022

    RF Coaxial Cable Assemblies are used in virtually all environments where wireless systems are deployed. Coaxial cable assemblies are integral internal parts of many wireless systems, and they are also used as interconnects between systems. These cable assemblies are often anywhere from a few inches long to hundreds of feet in length. This range of ..

    Read Full Article

    Power Added Efficiency (PAE) Calculator Explained

    12/01/2022

    RF power amplifiers typically have an input, output, and power supply rails. These rails can be either positive, negative, or dual positive and negative voltages. The input, output, and power supply rails all have recommended operating ranges of power, voltage, and current. This range is specified to nominal operation in what the manufacturer was able, ..

    Read Full Article

    Pasternack’s 50th Anniversary! An Interview with the Man who Started it all

    11/14/2022

    Pasternack has a milestone anniversary this year! Fifty years later, Pasternack products are as relevant and renowned as ever, and there’s no slowing down. To celebrate this momentous occasion, we recently had the opportunity take a trip down memory lane and learn the history of the brand from Murray Pasternack, the founder of Pasternack. Read ..

    Read Full Article

    Coaxial Cable Impedance Calculator

    11/03/2022

    The dominant use of coaxial cable in RF & Microwave applications is as a transmission line. Coaxial cables are extremely useful transmission lines as the coaxial nature of the transmission line provides relatively efficient transmission from DC to a cut-off frequency, which is a function of the geometries of the coaxial components of the cable. ..

    Read Full Article

    Antenna Downtilt & Coverage Calculator Chart

    10/20/2022

    An Antenna Downtilt and Coverage Calculator, or Antenna Tilt Calculator, aids the user by providing an approximate downward angle at which to install a directional antenna to reach desired signal strength and coverage between a transmitter and receiver at different heights and some distance away. An example use case is when a cell-tower directional transceiver ..

    Read Full Article

    Instant C to F Calculator: Convert Celsius to Fahrenheit in Seconds

    09/17/2022

    When it comes to temperature conversions, switching between Celsius and Fahrenheit can be confusing. Whether you’re traveling, cooking, or working on science projects, knowing how to convert Celsius to Fahrenheit (or vice versa) is crucial. That’s where an instant C to F calculator comes in handy. In this article, we’ll walk you through everything you ..

    Read Full Article

    All About RF Coaxial Connectors

    09/08/2022

      RF coaxial connectors are one of the most useful and ubiquitous methods of connecting RF systems and components. RF coaxial connectors are coaxial transmission lines made up of an RF coaxial cable and RF coaxial connectors terminating either end of the cable. RF connectors provide interconnect with other RF connectors, which must be of ..

    Read Full Article

    The Difference between RF Amplifier Types

    08/04/2022

    At first look, there are many different types of RF amplifiers, and it could be overwhelming to go from the specs you need to narrowing down what RF amplifier type is the best fit. Most RF amplifier types came about from the specification requirements of common transceiver, receiver, transmitter, radar, and modulation circuits and system-level ..

    Read Full Article
    Jump to of 31
    Live help