Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • RF Amplifier Power and Gain Considerations

    03/09/2017

    The input and output power characteristics of an RF amplifier are dominant characteristics, as increasing signal strength is the primary purpose of an amplifier. An RF amplifier will be specified with a maximum and nominal range for input and output power based on certain conditions. These specifications will further extend to a maximum and nominal ..

    Read Full Article

    RF Filter Overview – Types & Topologies

    03/02/2017

    RF filters are some of the most important components in receivers. The main functions of the filters are to reject undesirable signals outside the filter pass band and to separate signals according to their frequency. RF filters modify the amplitudes and phases of sinusoidal waveforms that pass through them or, more simply, RF filters remove unwanted ..

    Read Full Article

    Why Quality is Imperative for High Frequency Waveguides

    02/23/2017

    The quality of the construction and materials used can have a large impact on the performance of a waveguide system, especially in microwave frequencies and high power applications. This can become difficult to manufacture and evaluate, as the waveguide tolerances are extremely small at microwave and millimeter-wave frequencies. For instance, with millimeter-wave components and interconnects, ..

    Read Full Article

    Anatomy of a Coax Cable –and how they Work

    02/16/2017

    Coaxial cables are commonly known for being a broadband, relatively low-loss and high isolation transmission line technology. A coaxial cable is comprised of two concentric conductive cylinders separated by a dielectric spacer. The capacitance and inductance distributed along the coaxial line creates distributed impedance throughout the structure, known as characteristic impedance. The distributed resistive losses ..

    Read Full Article

    Antenna Gain and Directivity – The Basics

    02/09/2017

    What is antenna gain and directivity? Antennas, in essence, channel electrical power into electromagnetic signals. The shape, size, and connectorization all affect the antenna radiation pattern. Two key parameters in assessing the performance of an antenna are directivity and gain―directivity is a measurement of the concentration radiation in a direction while gain represents the power ..

    Read Full Article

    Directional Coupler and Power Divider/Combiner Overview

    02/02/2017

    Directional couplers are four port passive devices that employ an input port, output port, a port for the coupled signal and a port that is terminated internally. Directional couplers are used to couple a specific proportion of the power traveling in one transmission line out through another connection or port. Directional couplers are used in ..

    Read Full Article

    All About Jitter

    01/26/2017

    Though a detailed explanation of jitter can be highly complex mathematically, simply put, jitter is the deviation of a signal from its ideal periodic behavior in terms of frequency, signal amplitude, or phase. There are many contributors to jitter in a signal, from the source itself to outside interferers. Additionally, jitter can be described similarly ..

    Read Full Article

    5G Requirements

    01/19/2017

    Though no single 5G requirement is yet set in stone, there has been some consensus from various industrial partnerships, standards bodies, and regulatory agencies on a vision for 5G. Some aspects of this vision are debated as to when they may be realized, but a common timeframe is to have a full 5G definition with ..

    Read Full Article

    Fixed Attenuators 101

    01/12/2017

    RF attenuators are used to reduce the level of a signal. Some reasons why you might want to reduce the signal level would be to protect a circuit stage from receiving a signal that is too high or in applications where a signal level needs to be controlled. Attenuators typically consist of a resistive network ..

    Read Full Article

    Tips for Assembling, Troubleshooting and Handling Waveguides

    01/05/2017

    Though waveguide components and interconnects tend to be formed of relatively sturdy metals, some aluminum and copper waveguides, for higher frequency and aerospace applications, can easily be dinged and dented. Sometimes these dings and dents are a useful tuning technique; generally, they could dramatically change the performance of a waveguide or waveguide component. Ensuring that ..

    Read Full Article
    Jump to of 31
    Live help