Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • Directional Antennas Explained

    02/02/2026

    In reality, all types of RF antennas have some degree of directionality. However, there are certain antenna designs and types that are particularly directional compared to other antenna types. A Directional Antenna is useful in applications where it is desirable to receive a signal from a specific direction of origin or otherwise transmit a signal ..

    Read Full Article

    What Is the Difference Between Directional and Omnidirectional Antennas and What Are They Used For?

    05/16/2024

    Antennas are the basic components and devices used to convert electromagnetic signals traveling through free space to a conductive environment via waveguides and transmission lines. Antennas can be as simple as a single exposed conductor or as complicated as modern active/advanced antenna systems (AAS) with hundreds of individual antenna elements and active electronics driving each ..

    Read Full Article

    The Wide and Diverse World of RF Antennas

    07/14/2022

    Electromagnetic (EM) Antennas are an essential component for virtually all transmission and reception systems that operate in the RF, microwave, millimeter-wave (mmW), and terahertz (THz) frequency ranges. Another way to look at EM Antennas, is that these antennas can be designed to convert conducted EM signals to radiated EM signals, and vice versa, from kilohertz ..

    Read Full Article
    Jump to of 1
    Live help