Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • Difference Between Frequency Dividers and Power Dividers

    09/10/2020

    Though both often dubbed as “dividers”, frequency dividers and power dividers perform very different functions. Where a power divider splits an input signal power to two or more output ports, a frequency divider actually outputs a frequency that is a fraction of the input frequency. A frequency divider should not be confused with a diplexer ..

    Read Full Article

    Brief on Frequency Dependent Conductivity In Metallic Wires/Traces

    09/03/2020

    It has been understood for nearly a century that the conductivity of conductive metals changes as a function of frequency. Though this is the case the phenomenon behind frequency dependent conductivity is not as well understood by man. It was observed early on that the attenuation and resistive losses of metallic transmission lines and traces ..

    Read Full Article

    Why Hermetic Enclosures/Sealing?

    08/27/2020

    A hermetically sealed enclosure, or hermetic packaging, is a method of encapsulating a device or system in an environmentally protected package that prevents the exchange of the inside and outside environment. Hermetic packages are commonly seen in automotive, industrial, naval, military, and aerospace applications where the outside environment may lead to damage, early failure, or ..

    Read Full Article

    Harping on Harmonics

    08/20/2020

    Harmonics are spurious signal content (or spurious emissions) that are generated by a single frequency tone and nonlinear elements within a RF/microwave signal chain, or single-tone intermodulation distortion (IMD). The nonlinear elements create harmonics that are integer multiples of the fundamental frequency (often called the first harmonic). For instance, fo is the fundamental frequency and ..

    Read Full Article

    What Are Dynamic Range, SNR, P1dB, and Other Common RF/Microwave Characteristics

    08/13/2020

    There are several key methods of describing RF signal quality and device performance in respect to noise and linearity. As noise and linearity are often key considerations of both transmit and receive chains in communications and sensing systems, it is valuable for a technical professional to understand these parameters. The following is a brief description ..

    Read Full Article

    Low Noise Design and Device/Component Considerations

    08/06/2020

    It may be surprising to some that low power system and device/component design share many of the same considerations as high power system design, albeit for different reasons. The goal of low noise design is to limit the amount of added noise, harmonics, spurs, and other factors that increase the noise floor of a signal ..

    Read Full Article

    High Power RF/Microwave Considerations

    07/30/2020

    Like with other key RF/microwave component and device parameters, accounting for power extremes in RF design and system integration requires a nontrivial amount of additional considerations. If the RF signal is optimized for other performance factors, such as noise, linearity, phase noise, or other signal quality factors and the signal power is well within the ..

    Read Full Article

    Basics of Satellite Ground Station Hardware

    07/23/2020

    A ground station, earth station, or earth terminal is the terrestrial radio system used in extraplanetary telecommunications with spacecraft and satellites. Ground stations are used to communicate, bidirectionally, with satellites and spacecraft, or receive electromagnetic energy in the radio frequency spectrum from astronomical sources. Given the nature of extraplanetary communications, ground stations and satellites/spacecraft typically ..

    Read Full Article

    Using Cooling and Cryogenics to Reduce Noise Figure

    07/16/2020

    Ultra-sensitive systems depend on receiver components with as low an added noise figure as possible. Any added noise figure in the receiver chain reduces the signal-to-noise (SNR) of the receiver, and is cumulative. Hence, for each component in the receiver chain contributing noise, the noise floor of the receiver raises. A common method to reduce ..

    Read Full Article

    Basics of SAR and ISAR Radar – Radar Operation – Part 4

    07/09/2020

    Synthetic aperture radar (SAR) and inverse SAR (ISAR) are methods of using radar to map a stationary object, more usually terrain. SAR/ISAR systems are deployed on aircraft or satellites that move at high velocities in respect to the surface of the earth or potentially any stationary object or terrain. SAR/ISAR benefits from the phenomenon that ..

    Read Full Article
    Jump to of 38
    Live help