Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • Microwave Measurement Methods of Dielectrics

    05/06/2021

    Conductors, semiconductors, and insulators are the main building blocks of virtually all RF/microwave electronics. Insulators have dielectric properties that impact the electric fields that pass through them. In order to design an RF component or device, detailed knowledge of the dielectric properties of the insulators used in the construction of the component/device is essential. The ..

    Read Full Article

    Waveguide Amplifier Introduction & Applications

    04/29/2021

    Waveguide amplifiers are amplifiers specifically designed to be housed within a waveguide assembly. This provides some intrinsic advantages and trade-offs compared with coaxial connectorized amplifier assemblies or pallet amplifiers. Given that waveguide amplifiers are designed to directly mate with a given waveguide size and type, they are innately banded, as the waveguide has a limited ..

    Read Full Article

    RF Applications Series: Buried Object Detection Using Ground Penetrating Radar

    04/22/2021

    Ground penetrating radar (GPR) is a technology that uses pulses of electromagnetic energy sent into the ground to create reflections from the ground compositions and objects within the ground. These reflections can then be analyzed by software and turned into a plot or map projection so that objects within the ground can be identified or ..

    Read Full Article

    RF Component & Device Test Series: Coaxial Cable Assembly Performance Testing Part 2

    04/15/2021

    In part 1 of this series we delved into several of the commonly specified electrical performance characteristics for coaxial cable assemblies. This post wraps up the most common parameters: •  Capacitance •  Group Delay •  Velocity of Propagation •  RF Shielding/Leakage •  Maximum Input Power (Power Handling) •  Maximum Voltage/Breakdown Voltage •  Phase Stability (during ..

    Read Full Article

    RF Component & Device Test Series: Coaxial Cable Assembly Performance Testing Part 1

    04/08/2021

    In the previous post we explored quality testing of coaxial cable assemblies. In this post, we are exploring the electrical performance testing of coaxial cable assemblies. The following is a list of the most common electrical performance parameters given for coaxial cable assemblies. Key Coaxial Assembly Performance Tests • Frequency Range (Cutoff Frequency) • Insertion ..

    Read Full Article

    RF Component & Device Test Series: Coaxial Cable Assembly Quality Testing

    04/01/2021

    Coaxial cable assemblies are at the heart of many conductive interconnect solutions from the module level to complete systems. Coaxial cable assemblies are used in a wide array of applications from low-cost connection of consumer equipment to extreme precision and reliability needed in aerospace and satellite communications. From R&D to defense, coaxial cable assemblies are ..

    Read Full Article

    Where Are We With 6G?

    03/25/2021

    5G is just on the cusp of deployment, with most mobile networks still operating on 4G-LTE technology. So, is it a bit early to be talking about 6G? Given that telecommunications service providers and technology developers have somewhat settled on a new generation of cellular wireless technology every 10 years, this means that 6G is ..

    Read Full Article

    Updates on RF Silicon Technology

    03/18/2021

    Though Gallium Nitride (GaN) has been making headlines for the past several years as an emerging RF technology, RF semiconductors developed with silicon, namely RF silicon-on-insulator (RF-SOI), has also been advancing as a semiconductor of choice for the exploding RF hardware markets.  Where GaN is a still relatively expensive and small wafer technology, RF-SOI is ..

    Read Full Article

    RF/Microwave Test Equipment Useful for EMC Precompliance Testing

    03/11/2021

    Virtually every country around the world has some type of electromagnetic compliance (EMC) policy in place to prevent hazardous emissions, susceptible electronics in the marketplace, and to avoid an overabundance of interference. Given the complex nature of EMC, most compliance codes are very strict and the cost of failure is that a product cannot be ..

    Read Full Article

    Overview of High Power RF Attenuators

    03/04/2021

    RF Attenuators come in a wide variety of packages, technologies, and performance ranges. Some RF attenuator technology is compact enough to fit on an IC, while some units are large enough to require internal and/or external thermal management systems. The size and significance of the thermal management of an RF attenuator depends on the attenuator ..

    Read Full Article
    Jump to of 38
    Live help