Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • Directional Antennas Explained

    02/02/2026

    In reality, all types of RF antennas have some degree of directionality. However, there are certain antenna designs and types that are particularly directional compared to other antenna types. A Directional Antenna is useful in applications where it is desirable to receive a signal from a specific direction of origin or otherwise transmit a signal ..

    Read Full Article

    The Uses and Benefits of Omnidirectional Antenna Types

    10/08/2024

    In today’s interconnected world, omnidirectional antenna types have become essential tools for expanding connectivity. Ideal for both indoor and outdoor use, serve as reliable solutions for users who need wide-ranging signal coverage without the hassle of constant adjustments. Supporting applications from mobile networks to Wi-Fi connectivity, omni antennas provide the flexibility and dependable performance needed ..

    Read Full Article

    What Is the Difference Between Directional and Omnidirectional Antennas and What Are They Used For?

    05/16/2024

    Antennas are the basic components and devices used to convert electromagnetic signals traveling through free space to a conductive environment via waveguides and transmission lines. Antennas can be as simple as a single exposed conductor or as complicated as modern active/advanced antenna systems (AAS) with hundreds of individual antenna elements and active electronics driving each ..

    Read Full Article

    What Are Standard Gain Horn Antennas & Accessories Used For?

    03/07/2024

    A standard gain horn antenna is a type of waveguide antenna that is used in a variety of test/measurement, sensing, radar, and communications applications. Waveguide antennas, such as standard gain horns are used in these applications due to their high gain, efficiency, and precision performance. There are Standard Gain Horn Antennas With Waveguide Input and ..

    Read Full Article

    What Is A 2.4 GHz Antenna?

    01/25/2024

    There is a plethora of wireless communications antennas labeled as a 2.4 GHz antenna, this does not mean that these antennas only operate at exactly 2.4 GHz. It implies that they cover some area of the 2.4 GHz ISM band, which extends from 2.4 GHz to 2.5 GHz. In most cases, for the 2.4 GHz ..

    Read Full Article

    What Are Cellular, Wi-Fi, and GPS Combination IoT Antennas Useful For?

    10/26/2023

    Many of the latest Internet-of-Things (IoT) systems make use of multiple forms of wireless communication. In some cases, a single IoT module may be equipped with several wireless communication standards for various functions. For high bandwidth connections to infrastructure, cellular communications modules are common. For extremely high bandwidth and short range, or confined operation within ..

    Read Full Article

    The 2.4GHz Antenna: A Key to Reliable Wi-Fi and Bluetooth Performance

    04/16/2023

    Antennas operating at 2.4 GHz are critical to modern wireless communications. Whether you’re setting up Wi-Fi in your home, syncing your Bluetooth devices, or controlling your drone, a 2.4GHz antenna plays an indispensable role. These antennas are widely adopted for their balance between range and data transmission capabilities, supporting technologies like Wi-Fi, Bluetooth, and Zigbee, ..

    Read Full Article

    What are the common very high frequency/ultra-high frequency (VHF/UHF) [30 MHz to 300 MHz, and 300 MHz to 1000 MHz] antenna types?

    02/02/2023

    VHF/UHF stands for very high frequency and ultra-high frequency, respectively. These frequency designations are in both the ITU and IEEE radar bands, but in this case we are discussing IEEE radar bands VHF and UHF, 30 MHz to 300 MHz and 300 MHz to 1000 MHz in the US. This is an important note, as ..

    Read Full Article

    Antenna Downtilt & Coverage Calculator Chart

    10/20/2022

    An Antenna Downtilt and Coverage Calculator, or Antenna Tilt Calculator, aids the user by providing an approximate downward angle at which to install a directional antenna to reach desired signal strength and coverage between a transmitter and receiver at different heights and some distance away. An example use case is when a cell-tower directional transceiver ..

    Read Full Article

    The Wide and Diverse World of RF Antennas

    07/14/2022

    Electromagnetic (EM) Antennas are an essential component for virtually all transmission and reception systems that operate in the RF, microwave, millimeter-wave (mmW), and terahertz (THz) frequency ranges. Another way to look at EM Antennas, is that these antennas can be designed to convert conducted EM signals to radiated EM signals, and vice versa, from kilohertz ..

    Read Full Article
    Jump to of 3
    Live help