Global Positioning System (GPS) and Global Navigation Satellite System (GNSS) technologies are fundamental to modern navigation, positioning and timing systems. UAV platforms, autonomous vehicles, defense systems and surveying equipment all rely on accurate GNSS signals to determine precise location and maintain mission awareness.
However, GNSS performance can degrade significantly in contested or challenging environments. Weak satellite signals must travel long distances before reaching receivers, making them vulnerable to interference, obstructions and atmospheric disruptions. When these signals are degraded or blocked, positioning accuracy can decline rapidly.
High-gain antennas play an important role in restoring reliable GNSS performance. By improving signal strength and enhancing signal-to-noise ratio, these antennas help receivers maintain stable positioning even in complex RF environments.
Key Takeaways
- • GPS and GNSS systems depend on extremely weak satellite signals that are vulnerable to disruption
- • Contested environments introduce interference, signal reflections and physical obstructions
- • GNSS accuracy is critical for UAV navigation, surveying and mission-critical positioning
- • High-gain antennas improve signal reception and increase signal-to-noise ratio
- • Pasternack supports GNSS system reliability with high-performance RF antennas and interconnect solutions
Understanding GPS/GNSS Technology and Its Importance
GPS and GNSS technologies determine location by receiving signals from multiple satellites orbiting the Earth. Each satellite transmits precise timing and positioning information that receivers use to calculate geographic coordinates.
These systems enable a wide range of applications including aviation navigation, surveying, logistics tracking and UAV guidance. Accurate positioning allows systems to maintain safe flight paths, map terrain, coordinate operations and deliver precise navigation data.
Because GNSS signals originate from satellites more than 20,000 kilometers above Earth, they arrive at receivers extremely weak. This makes the quality of signal reception critical for maintaining positioning accuracy.
Understanding GPS/GNSS Accuracy
GPS/GNSS accuracy refers to how closely a receiver’s calculated position matches its true geographic location. Accurate positioning depends on reliable signal reception from multiple satellites.
Several factors influence GNSS accuracy under normal conditions. Satellite geometry affects how signals intersect at the receiver, which can influence positioning precision. Receiver quality and antenna performance also affect how effectively signals are captured and processed.
Accuracy is especially important in applications where precise positioning is required. UAV navigation, surveying operations, mapping systems and defense missions all depend on reliable location data to operate safely and effectively.
Challenges in Contested Environments
Contested environments introduce additional challenges that can significantly degrade GNSS signal quality.
These environments may include dense urban areas, mountainous terrain, forests or regions where intentional electronic interference is present. Each of these conditions can affect signal propagation and reduce positioning accuracy.
Signal Interference
GNSS signals operate at low power levels and can be easily disrupted by electromagnetic interference. Intentional jamming or spoofing attempts can overwhelm receiver inputs and prevent accurate signal interpretation.
Unintentional interference from nearby electronic systems may also degrade signal quality.
Multipath Effects
Multipath occurs when satellite signals reflect off buildings, terrain or other structures before reaching the receiver. These reflected signals arrive later than direct signals, introducing timing errors that affect position calculations.
Urban environments are particularly prone to multipath interference due to reflective surfaces such as buildings and infrastructure.
Physical Obstructions
Natural and man-made obstacles can block satellite signals entirely. Buildings, mountains and dense vegetation may prevent receivers from accessing enough satellite signals to calculate an accurate position.
When fewer satellites are visible, GNSS receivers may experience reduced accuracy or intermittent signal loss.
Atmospheric Conditions
The ionosphere and troposphere can also affect GNSS signal propagation. Variations in atmospheric conditions may introduce signal delays that affect positioning calculations.
Although many receivers compensate for these effects, severe atmospheric disturbances can still reduce accuracy.
The Role of High-Gain Antennas
High-gain antennas help improve GNSS reception by increasing the strength of incoming satellite signals. These antennas focus reception toward signals arriving from satellites, improving the receiver’s ability to capture weak signals.
By improving signal-to-noise ratio, high-gain antennas help GNSS receivers distinguish legitimate satellite signals from background noise or interference.
Improved signal quality allows receivers to maintain stable satellite lock even in environments where signal strength is reduced or interference is present.
In UAV systems and other mission-critical platforms, high-gain antennas provide an important layer of resilience for GNSS navigation systems.
Best Practices for Using High-Gain Antennas
To maximize GNSS performance, high-gain antennas must be properly integrated into the RF system.
Proper antenna placement is critical. Antennas should be positioned with clear visibility of the sky to maximize satellite signal reception. Obstructions near the antenna can reduce performance and introduce multipath effects.
Low-loss RF cables and connectors should also be used to preserve signal strength between the antenna and receiver. Excessive insertion loss in the RF chain can reduce the benefits provided by high-gain antennas.
Careful integration of antennas, cables and receivers ensures GNSS systems maintain optimal performance even in challenging environments.
Improving GNSS Reliability in Challenging RF Environments
Maintaining accurate GNSS positioning in contested environments requires a system-level approach to RF design. High-gain antennas play a central role by strengthening incoming satellite signals and improving receiver sensitivity.
When combined with low-loss cables, high-quality connectors and proper filtering, these antennas help GNSS systems maintain stable positioning performance even when signal conditions are less than ideal.
Pasternack supports engineers with high-performance RF antennas, cables and microwave components designed to enhance GNSS reliability across aerospace, defense and UAV applications.
Learn more about RF solutions designed to support reliable UAV communication, navigation and mission-critical connectivity in aerospace and military environments.
Explore Pasternack UAV Solutions
Frequently Asked Questions
Why are GPS/GNSS signals vulnerable in contested environments?
GNSS signals are extremely weak when they reach Earth and can be easily disrupted by jamming, spoofing or electromagnetic interference.
How do high-gain antennas improve GNSS performance?
High-gain antennas increase signal strength and improve signal-to-noise ratio, allowing receivers to maintain stronger satellite connections and more accurate positioning.
Can antenna upgrades alone prevent GNSS disruption?
High-gain antennas significantly improve signal reception, but complete RF chain optimization—including low-loss cables, connectors and filtering—helps ensure maximum resilience in challenging environments.