Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • Directional Antennas Explained

    02/02/2026

    In reality, all types of RF antennas have some degree of directionality. However, there are certain antenna designs and types that are particularly directional compared to other antenna types. A Directional Antenna is useful in applications where it is desirable to receive a signal from a specific direction of origin or otherwise transmit a signal ..

    Read Full Article

    What are the common very high frequency/ultra-high frequency (VHF/UHF) [30 MHz to 300 MHz, and 300 MHz to 1000 MHz] antenna types?

    02/02/2023

    VHF/UHF stands for very high frequency and ultra-high frequency, respectively. These frequency designations are in both the ITU and IEEE radar bands, but in this case we are discussing IEEE radar bands VHF and UHF, 30 MHz to 300 MHz and 300 MHz to 1000 MHz in the US. This is an important note, as ..

    Read Full Article
    Jump to of 1
    Live help