Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • SMA Connector Overview

    12/29/2022

    SMA Coaxial Connectors, or just SMAs, are one of the most common coaxial connector types used throughout the RF, microwave, and even millimeter-wave (mmW) industries. SMA stands for subminiature version A and was developed in the 1960s. The interface dimensions and other aspects of the SMA connector are detailed in MIL-STD-348 and was originally designed ..

    Read Full Article

    Introduction to RF/Microwave Launch Accessories & Field Replaceable Connectors

    06/02/2022

    Many RF/microwave applications use connectorized modules that are hermetically or otherwise sealed to protect sensitive internal electronics from the elements. In some rugged applications, such as military, aerospace, industrial, and telecommunications, the exposed connectors on these modules can become corroded or otherwise damaged during regular use. This is especially true if the external connectors are ..

    Read Full Article
    Jump to of 1
    Live help