Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • Signal Chain Discussion Series: Local Oscillators

    12/17/2020

    A local oscillator (LO) is an electronic oscillator that generates a very narrow bandwidth signal, or tone, with high purity and stability for use in frequency conversion circuits and timing. As the performance of frequency conversion circuits and timing systems are often dependent on the LO performance, the quality of the oscillator and LO electronic ..

    Read Full Article

    5G Oscillators Requirements Soar In the Wake of Stringent Timing & Synchronization Requirements

    06/18/2020

    Though 5G comes with many promises of a ubiquitous high-speed experience with dramatically improved performance over 4G systems, there are several necessary upgrades to underlying technology and infrastructure that are necessary to achieve those desired ends. One such area is with timing and synchronization. In order to realize the desired 5G network responsiveness for high ..

    Read Full Article

    An Introduction to Phase-Locked-Loops and RF Oscillators

    12/20/2018

    In most RF systems, the production, transmission, and reception of a radio frequency signal is accomplished by way of a transmitter which amplifies and modulates the signal and a receiver system which feeds the signal into the mixer circuits to enable frequency conversion and demodulation. An oscillator is a circuit that generates a repetitive waveform, ..

    Read Full Article
    Jump to of 1
    Live help