Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • RF Applications Series: Buried Object Detection Using Ground Penetrating Radar

    04/22/2021

    Ground penetrating radar (GPR) is a technology that uses pulses of electromagnetic energy sent into the ground to create reflections from the ground compositions and objects within the ground. These reflections can then be analyzed by software and turned into a plot or map projection so that objects within the ground can be identified or ..

    Read Full Article

    Basics of SAR and ISAR Radar – Radar Operation – Part 4

    07/09/2020

    Synthetic aperture radar (SAR) and inverse SAR (ISAR) are methods of using radar to map a stationary object, more usually terrain. SAR/ISAR systems are deployed on aircraft or satellites that move at high velocities in respect to the surface of the earth or potentially any stationary object or terrain. SAR/ISAR benefits from the phenomenon that ..

    Read Full Article

    Basics of Chirp Radar – Radar Operation – Part 3

    06/11/2020

    Chirp Radar is a type of radar that uses frequency modulation and pulse compression (which may confuse many as chirp has also been used as a synonym for “pulse compression”), which combines the capabilities of frequency modulation and pulse radar. Some of the benefits of a Chirp radar over a simple pulse radar are range ..

    Read Full Article

    Basics of FMCW Radar – Radar Operation – Part 2

    06/04/2020

    A continuous wave (CW) Doppler radar can be augmented via the use of frequency modulation. This type of radar is known as a frequency modulated continuous wave (FMCW) radar. The use of frequency modulation allows for the detection of both range and target velocity, as well as the ability to discriminate between multiple targets. A ..

    Read Full Article

    Basics of Pulse Radar – Radar Operation – Part 1

    05/28/2020

    A pulsed radar is a sensing system that uses a high power pulsed signal reflected off of objects to determine their distance from the radar antenna. The basic operation of a pulse radar is that a pulse modulator generates a short pulsed which is then amplified. The amplified pulse then passes through a duplexer or ..

    Read Full Article
    Jump to of 1
    Live help