Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • Signal Chain Discussion Series: Basic Pulsed Radar Front-End Amplifiers

    10/08/2020

    Pulsed radar are used in a variety of applications for weather sensing, marine sensing, aerospace navigation, and defense. Critical to pulsed radar performance is the behavior of the radar’s RF front-end hardware. Though pulse radars have advanced significantly in the past several years, with deep digital integration, the RF front-end hardware of these radars is ..

    Read Full Article

    Basics of Pulse Radar – Radar Operation – Part 1

    05/28/2020

    A pulsed radar is a sensing system that uses a high power pulsed signal reflected off of objects to determine their distance from the radar antenna. The basic operation of a pulse radar is that a pulse modulator generates a short pulsed which is then amplified. The amplified pulse then passes through a duplexer or ..

    Read Full Article
    Jump to of 1
    Live help