Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • When DAS Meets PIM: On the Challenges of Accounting for PIM with Distributed Antenna Installations (Part 2)

    04/11/2019

    In last week’s post, we covered foundational details regarding PIM in modern wide-band and multi-carrier communication systems, with a note on upcoming 5G NR sub-6 GHz frequencies being added to the mix. This week’s blog expands upon that discussion and provides more details of PIM considerations specific to DAS. With DAS, another large PIM concern ..

    Read Full Article

    When DAS Meets PIM: On the Challenges of Accounting for PIM with Distributed Antenna Installations (Part 1)

    04/04/2019

    Passive intermodulation distortion is the result of discontinuities, metal-to-metal contact, and material properties that lead to nonlinear characteristics of typically linear passive transmission lines and components. PIM can be induced in a variety of RF components, such as connectors, adapters, cable, combiners, splitters, couplers, tappers, attenuators, terminators, antennas, and cable-to-board interconnect. PIM is generated when ..

    Read Full Article

    Coaxial Cable Assemblies Aren’t the Only Low PIM Devices (Tappers, Splitters, Couplers, Loads, Adapters, and Antennas) Part 2

    03/28/2019

    Last week’s post covered why low PIM components, other than coaxial cables and assemblies, can be important to consider for low PIM applications. This blog focuses on low PIM Directional Couplers, Loads, Attenuators, Adapters, and Antennas, and provides brief descriptions of their use cases and value. Low PIM Directional Couplers Unlike tappers, splitters, and dividers, ..

    Read Full Article

    What is so Special About the 4.3-10 Coaxial Connector?

    04/05/2018

    There are many coaxial connectors used in wireless and wired networks, including DIN 7/16, N, 4.1/9.5, and the 4.3-10 interface. Typically, the choice of a connector boils down to economics, power handling, size, and installation criteria. However, the increasing number of wireless network bands and mobile data rates pose a very stringent requirement for transmission ..

    Read Full Article
    Jump to of 1
    Live help