Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • What Is A RF Amplifier, And What Are They Used For?

    10/17/2024

    Within an RF signal chain, there is often the need to provide some signal conditioning in incoming, outgoing, or through signals. One of the most needed signal conditioning methods is amplification of signal energy, which is the key function of RF Amplifiers. Signal amplification involves increasing the amplitude of a signal, this could imply voltage, ..

    Read Full Article

    Harnessing the Potential of the 110 MHz Frequency with Broadband Amplifiers

    02/27/2024

    Whether used in communication networks, broadcasting systems, or advanced testing environments, the 110 MHz frequency requires precision tools to amplify signals and minimize interference. In communication networks, broadcasting systems, or advanced testing environments, this frequency requires precision tools to amplify signals and minimize interference. Tools like 110 MHz frequency broadband amplifiers ensure seamless signal transmission ..

    Read Full Article

    The Difference between RF Amplifier Types

    08/04/2022

    At first look, there are many different types of RF amplifiers, and it could be overwhelming to go from the specs you need to narrowing down what RF amplifier type is the best fit. Most RF amplifier types came about from the specification requirements of common transceiver, receiver, transmitter, radar, and modulation circuits and system-level ..

    Read Full Article
    Jump to of 1
    Live help