Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • What is Plenum Rated Coaxial Cable?

    12/21/2023

    It is important for any installer, communications technician, and acquisition personnel to understand the purpose of “fire rated cables”, as lives are literally on the line. In the United States, the National Fire Protection Association (NFPA) outlines standards for in-building electrical wiring that are located in the National Electrical Code (NEC). Though the NEC isn’t ..

    Read Full Article

    Does Matter for Smart Homes Matter for RF Hardware?

    12/07/2023

    This year, an increasing number of smart home devices are being shipped and marketed as Matter certified. Many of these smart home devices are wireless Internet-of-Things (IoT) devices, which begs the questions: is Matter a relevant wireless standard, and does it/will it impact the wireless hardware in smart home IoT devices along with subsequent hardware ..

    Read Full Article

    Wi-Fi Next Generation (Wi-Fi 7) Updates

    11/23/2023

    The next generation of Wi-Fi, IEEE 802.11be, or Wi-Fi 7 standard, is slated to be officially released in early 2024. However, there are already a host of devices on the market that are touting Wi-Fi 7 capabilities, as early drafts of the standard have been regularly released as the amendment has been developed. This means ..

    Read Full Article

    What is a D-Sub Connector/Contact?

    11/09/2023

    D-Sub, or D-Subminiature, connectors are used in a variety of applications from military/defense to commercial technology and computer/networking technology. D-Sub connectors can be used for power, analog, RF, or digital signal transmission, and are often readily repaired/replaced/installed in the field. This connector style is extremely versatile and can be found anywhere from temperature-controlled data centers ..

    Read Full Article

    Why 2.4mm Connectors Are the Backbone of High-Frequency, Eco-Compliant RF Systems

    11/05/2023

    In the world of RF and microwave engineering, 2.4mm connectors are indispensable, particularly in high-frequency and precision applications. Designed with a focus on handling high-frequency signal applications, these RF connectors are key to industries that require low-loss signal integrity and robust connectivity, such as telecommunications, aerospace, and advanced research labs. Because they also satisfy stringent ..

    Read Full Article

    What Are Cellular, Wi-Fi, and GPS Combination IoT Antennas Useful For?

    10/26/2023

    Many of the latest Internet-of-Things (IoT) systems make use of multiple forms of wireless communication. In some cases, a single IoT module may be equipped with several wireless communication standards for various functions. For high bandwidth connections to infrastructure, cellular communications modules are common. For extremely high bandwidth and short range, or confined operation within ..

    Read Full Article

    Why a Centigrade and Fahrenheit Converter Matters for RF, Microwave, and mm-Wave Applications

    10/12/2023

    A Centigrade and Fahrenheit converter is an essential tool in the world of RF, microwave, and millimeter-wave engineering. It’s a world where temperature stability is crucial to the performance of both active and passive components, and a Centigrade and Fahrenheit converter can help ensure such stability. Whether you’re working with antennas, amplifiers, or oscillators, understanding ..

    Read Full Article

    Deciphering TRB, TRT, TRS, TTM, TRC, TRN, TWBNC, TWTNC, Triax, Twinax, and other coaxial and triaxial connector terms

    09/28/2023

    As is common in many industries, there are often internal acronyms or company part names/standards that may eventually spread to the larger industry. This is the case for some of the types of twinaxial and triaxial transmission line components, such as TRB Plug to TRB Jack Right Angle Adapters, that are present in the RF ..

    Read Full Article

    Everything You Need to Know About the Female to Female Coax Adapter in Modern Connectivity

    09/24/2023

    When it comes to multimedia and communications, ensuring your signal runs smooth is paramount. A female to female coax adapter serves as a crucial component in achieving this, especially when you’re dealing with coaxial cable setups. Whether you’re looking to connect multiple video devices, extend a pre-existing connection, or simply need a quick fix for ..

    Read Full Article

    What Are High Voltage (HV) Coaxial Connectors, Cables, & Cable Assemblies?

    09/14/2023

    There are several high voltage (HV) applications, such as in instrumentation, imaging inspection, medical, aerospace, and military/defense that pose the problem of connecting high voltage power supplies, signal generators, and instruments to devices-under-test (DUTs) and other equipment. High quality coaxial connectors and cables are naturally well suited to carrying low to medium voltages, and there ..

    Read Full Article
    Jump to of 38
    Live help