Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • Introduction to MIL-PRF-39012 and MIL-STD-348 Coaxial Connectors

    02/02/2026

    To enable interoperability amongst RF systems, the military and industry rely on standardized dimensions and types of coaxial connectors. The two major standards that define coaxial connectors for the US military are MIL-STD-348 and MIL-PRF-39012. MIL-STD-348 provides the dimensions for control of the standard interfaces, while MIL-PRF-39012 defines the, detail specifications, materials, quality conformance, qualification, ..

    Read Full Article

    What’s the Difference Between a Diplexer and a Duplexer?

    RF Diplexers and Duplexers are very common RF components in transmitters, receiver, and transceiver circuits for communications, radar, and other sensing applications. As the terms are similar, they are sometimes mistakenly used interchangeably, which isn’t appropriate. Diplexers and Duplexers perform very different functions, though they are located in similar areas in a circuit block diagram. ..

    Read Full Article

    CW Power Capacity vs Frequency (Electromechanical Switches)

    RF Electromechanical Relay Switches, RF electromechanical switches, or RF electromechanical relays are a type of RF switch with mechanical contacts driven by electrically driven actuators. The transmission paths within an Electromechanical relay switch are purely passive, and thus exhibit relatively low loss and high isolation compared to active switch technologies. Due to the low loss ..

    Read Full Article

    RF Cables vs Fiber Optic Cables | Key Differences & Best Applications

    09/16/2025

    In the world of high-speed communication and signal transmission, choosing the right medium can make or break system performance. Two of the most widely used transmission technologies—RF (Radio Frequency) cables and fiber optic cables—serve distinct roles in modern infrastructure. Whether you’re designing a wireless backhaul, a satellite ground station, or a data center interconnect, understanding the strengths and limitations of each ..

    Read Full Article

    Ensuring Reliability in Space-Grade RF Coaxial Interconnects

    05/30/2025

    In the unforgiving environment of space, RF coaxial interconnects must meet rigorous demands for performance, durability, and consistency. From extreme temperature fluctuations to high levels of radiation and vibration, these components are essential to mission success. In our latest article for Microwave Journal, Pasternack explores the essential design and material considerations for building space-grade RF ..

    Read Full Article

    New White Paper Explores MIL-DTL-38999 Connector Essentials

    05/13/2025

    Designing for Harsh Environments? Start with MIL-DTL-38999.  Pasternack’s latest technical resource, “Primer on MIL-DTL-38999 Connectors and Contacts,” offers engineers and designers a comprehensive overview of one of the most trusted interconnect standards used in military, aerospace, and high-reliability environments. This detailed white paper explores the evolution of the MIL-DTL-38999 standard, connector series types (I–IV), materials ..

    Read Full Article

    What Is A RF Amplifier, And What Are They Used For?

    10/17/2024

    Within an RF signal chain, there is often the need to provide some signal conditioning in incoming, outgoing, or through signals. One of the most needed signal conditioning methods is amplification of signal energy, which is the key function of RF Amplifiers. Signal amplification involves increasing the amplitude of a signal, this could imply voltage, ..

    Read Full Article

    The Uses and Benefits of Omnidirectional Antenna Types

    10/08/2024

    In today’s interconnected world, omnidirectional antenna types have become essential tools for expanding connectivity. Ideal for both indoor and outdoor use, serve as reliable solutions for users who need wide-ranging signal coverage without the hassle of constant adjustments. Supporting applications from mobile networks to Wi-Fi connectivity, omni antennas provide the flexibility and dependable performance needed ..

    Read Full Article

    RF Low Noise Amplifiers (LNAs) Applications & Considerations

    10/03/2024

    Throughout the signal chain and especially at a signal input stage, RF signals for communications and sensing can be extremely weak. RF Low Noise Amplifiers (LNAs) are the most common method for increasing the signal level of these very weak signals while minimizing the introduction of signal degrading factors. Of these signal degrading factors, added ..

    Read Full Article

    What Is High Gain and How Does It Impact Amplifier Performance?

    09/19/2024

    RF sensing and communication applications often involve very weak signal levels. It is often necessary to use RF Amplifiers to increase the gain, or signal level, of these signals in order to digitize them or otherwise condition these signals to usable levels. However, there are a few trade-offs to consider when increasing a signal’s power ..

    Read Full Article
    Jump to of 38
    Live help