Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • Constraints and Considerations for Bi-directional Amplifiers

    08/31/2017

    Bi-directional amplifiers are used to strengthen communication signals between two points for a wide array of applications. This include boosting signals along large subterranean or in-building distributed antenna systems (DAS), acting as a repeater to a remote observation station, and even enabling rapidly deployable portable networks with unmanned aerial vehicles (UAVs). As many modern uses ..

    Read Full Article

    Waveguide Preventative Maintenance

    08/24/2017

    Though many failure modes cannot be predicted or avoided, many of the common failure modes of waveguide assemblies can be avoided by properly accounting for the applications demands and running preventative maintenance programs. If the outer coating/jacket of a waveguide cable run is important in preventing environmental ingress, visual and chemical inspections can be performed ..

    Read Full Article

    Introduction to RF Baluns

    08/17/2017

    A balun, meaning balanced-unbalanced, is a three-port device that converts differential signals to single-ended signals, and vice versa. Hence, a balun presents a 180° phase shift between the signals in the balanced end, unlike a power divider with no phase shift between the splitting ports. This functionality allows for baluns to take the input, or ..

    Read Full Article

    12 Tips and FAQs for Selecting the Right Coaxial Cable

    08/10/2017

    The growth of wireless and high speed data applications has only expanded the use of coaxial cabling beyond traditional video and telecommunications uses. With the growth and standardization of coaxial cabling for a wide range of applications, coaxial cabling has become very familiar in the home, office, telecommunication facility, rail platform, industrial plant, and government/public ..

    Read Full Article

    What you need to Consider When Selecting an Attenuator

    08/03/2017

    A systems engineer will often weigh many factors when selecting the appropriate attenuator for a specific application. An application may demand greater electrical, physical, or environmental properties from an attenuator and these factors will ultimately dictate the design constraints that lead to attenuator selection. The main electrical parameters considered, are the attenuation level and how ..

    Read Full Article

    Benefit of Millimeter-wave Development Systems

    07/27/2017

    The next generation of mobile wireless technologies (5G), RF imaging, and even radar will be leveraging upper microwave and millimeter-wave frequencies for high data rate communications and sensing applications. The U.S. FCC and ITR have already investigated several upper microwave and millimeter-wave bands for use for these applications, and intense international investment has been gaining ..

    Read Full Article

    Coax or Waveguide Interconnect? Which one should you use?

    07/20/2017

    Depending upon the frequencies, power levels, and physical requirements, either coaxial or waveguide interconnects are used for high power RF and Microwave applications. Both technologies vary in size as a function of frequency and require higher precision materials and manufacturing processes to handle higher power levels. Generally, as a product of the way the RF ..

    Read Full Article

    Understanding Key Mixer Performance Parameters

    07/13/2017

    A Radio Frequency mixer is a three-port passive or active device that combines two or more signals into one or two composite output signals, and is the backbone of heterodyne and superheterodyne communications technologies. The purpose of a mixer is to produce a signal at a new frequency, while preserving other characteristics of the initial ..

    Read Full Article

    Bi-Directional Amplifiers -Just the Facts

    06/29/2017

    A Bi-Directional amplifier (BDA) is a device that locates a wireless signal, amplifies it, and then rebroadcasts it throughout a building or area. The backbone of most range or signal extending technologies is a relatively simple dual amplifier device with an integrated low noise amplifier (LNA) and power amplifier (PA). The Bi-Directional amplifier either enables ..

    Read Full Article

    Waveguide Mechanical and Machining Considerations

    06/22/2017

    Waveguides are predominantly constructed entirely with conductive metals, with the exception of pressure windows, some gaskets  and jacketing materials. Generally, this means that waveguides are constructed in machining facilities by technicians knowledgeable in waveguide construction. Some of this knowledge is based in physics, such as the proper bend radius and lengths of bends, and some ..

    Read Full Article
    Jump to of 37
    Live help