Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • When Do You Need a Bias Tee or DC Block?

    11/16/2017

    Bias Tees and DC blocks are both low frequency filters designed to pass certain wanted signals and power rails while blocking other signals and limiting the performance impact on RF/microwave circuits. Bias Tees are essentially diplexers with an extremely low crossover frequency, and DC blocks are high pass filters with cutoff frequency down to audio ..

    Read Full Article

    Tips on Selecting a Frequency Divider or Frequency Multiplier

    11/09/2017

    Frequency translation is the backbone of superheterodyne communications and radar circuits, as well as many other useful RF/microwave devices. There is often confusion surrounding these nonlinear devices, specifically the role of mixers, multipliers, and dividers, and how to select the best device for an application. This post aims to briefly describe the similarities and differences, ..

    Read Full Article

    Directional Coupler Do’s and Don’ts

    11/02/2017

    Directional couplers are extremely useful passive RF components capable of extracting a small portion of the energy from the main transmission path, and redirecting it to one, or more, coupled ports. As isolation from the coupled ports to the main transmission path is desirable, directional couplers typically have high isolation among the ports. There are ..

    Read Full Article

    Let’s be Open with a Load of Info about Coaxial Calibration Kits

    10/26/2017

    Coaxial calibration kits (Cal-kits), or vector network analyzer (VNA) coaxial calibration kits, are indispensable tools for ensuring that a VNA is providing the most accurate measurements possible. Without regularly calibrating a VNA with quality termination components, the conditions in which a device under test (DUT) is testing will also be included in the test data. ..

    Read Full Article

    How to Accessorize Your Coaxial Cable and Connector

    10/12/2017

    In the case of test and measurement, cable and connector installations, and coaxial assemblies, there is substantial design effort and thought dedicated to selecting the optimal coaxial cables and connectors for the project. These factors include electrical properties, mechanical properties, infrastructure logistics, pricing, environmental ratings, and standards and qualifications. However, there is more to a ..

    Read Full Article

    The Basics of Frequency Synthesizers and Oscillators

    10/05/2017

    Modern transmitters and receivers leverage oscillators and frequency synthesizers to generate carrier signals, upconversion/downconversion local oscillator frequencies, aid in frequency tuning, and more. There are many different types of materials and technologies used in precision frequency generation. This post will provide a brief explanation of the different types of oscillators and frequency synthesizers common in ..

    Read Full Article

    EMC, EMI, and Environmental MIL-SPEC Standards That Affect RF Electronics

    09/28/2017

    As virtually all electronic systems—and even some mechanical, biological and chemical systems—are susceptible to electrostatic discharge (ESD), and when operating alongside other electronics there is a need for electromagnetic compatibility (EMC) standards. The DoD offers a handbook and several standards which cover ESD and EMC. MIL-HDBK-263 provides much of the background around the application of ..

    Read Full Article

    Flexible Waveguides Solve Difficult Application Challenges

    09/21/2017

    In many installations and test bench scenarios, a precisely designed rigid waveguide structure with the proper flange and orientation is not readily available. Lead times of several weeks to months are common to receive the correct part. This is not always convenient in a design, repair, or replacement situation. Flexible waveguides at various lengths enable ..

    Read Full Article

    RF Switch Configuration Options

    09/14/2017

    RF switches are broken down into several configurations, typologies, and technologies. The simplest distinction is the normally open-circuit or normally closed-circuit configurations. Generally, if unlabeled, a switch is normally open-circuit, though it is worth investigating to a high degree of confidence. If a switch remains in the switched state after power has been removed, the ..

    Read Full Article

    What’s the Hype with High-Reliability (Hi-Rel)

    09/07/2017

    It is common to see high reliability (Hi-Rel) labelled electronic components and devices in virtually every automotive, industrial, avionics, military, and space application. Obviously, these applications have widely different standards and expectations for reliability. For example, an automotive device may have an expected failure rate over 5 years that is orders of magnitude less than ..

    Read Full Article
    Jump to of 37
    Live help