Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • RF Test Equipment Series: Calibration Kits

    10/24/2019

    RF calibration kits are a key tool in ensuring that Vector Network Analyzer (VNA) and other RF instruments provide accurate measurements to the testing plane of the device. Due to the intrinsic addition of phase and impedance variation over RF test equipment interconnect, measurements from a VNA made without calibration will include the S-parameter and ..

    Read Full Article

    Introduction to Electromagnetic Compliance and Precompliance Testing

    10/17/2019

    Electromagnetic Compliance (EMC) and Precompliance Testing are methods of ensuring that electronic devices don’t overly emit unwanted electromagnetic (EM) radiation or electrical fields and are adequately immune to external EM radiation or electrical fields. There are specific EMC standard that Countries and regions require to be passed before products can be legally sold in those ..

    Read Full Article

    What Are OTA Ranges, Chambers, and Outdoor Far-Field Test Ranges?

    10/10/2019

    An essential method of testing communications and radar equipment is the use of Over-the-air (OTA) testing. OTA testing is performed on antenna, user equipment, base station equipment, satellite communication, ground station, radios, and radar for virtually all applications. Though extensive characterization testing and quality testing can be performed in a compact and automated testing rigs ..

    Read Full Article

    RF Test Equipment Series: Noise Sources/Noise Generators

    10/03/2019

    RF designers and engineers spend a significant amount of design and effort dealing with noise in RF systems. So, it surprises some that there is a whole branch of RF test equipment that’s sole purpose is to generate noise. Noise sources are a key piece of test equipment, as well as being integral parts of ..

    Read Full Article

    RF Test Equipment Series: Matrix Switches and Switch Matrices

    09/26/2019

    Matrix Switches, or Switch Matrices, are devices that enable the routing of RF signals through selectable paths. These devices can be as simple as single-input with two selectable outputs or as complex as having tens of inputs and outputs that can all be interested as needed. Switch Matrices are often used in test equipment setups ..

    Read Full Article

    RF Test Equipment Series: Signal Generators

    09/19/2019

    An RF Signal Generator is another keystone piece of RF test and measurement equipment, alongside spectrum analyzers and network analyzers. The purpose of signal generators is to create RF signals at varying power levels, frequencies, and in the case of vector signal generators, with various phase and waveform characteristics. RF signal generators are used in ..

    Read Full Article

    RF Test Equipment Series: Network Analyzers

    09/12/2019

    Network Analyzers, and Vector Network Analyzers (VNAs), are one of the cornerstone RF test instruments, and virtually every test center or lab usually employs some type of VNA. These test instruments are able to send electromagnetic energy into a component, device, antenna, assembly, etc. and accurately measure the power transmitted and reflected through the device-under-test ..

    Read Full Article

    Introduction to RF & Microwave Substrates & Base Materials

    09/05/2019

    The term “substrate” can be somewhat confusing the context of RF/Microwave devices, components, and applications. A substrate can generally be anything from the insulative material used to develop a semiconductor or film (thick-film or thin-film circuits or components), or the structural material of printed circuit boards (PCBs). These electrically insulating materials are the backbone of ..

    Read Full Article

    Roundup of RF Transistor Types, Semiconductors, and Configurations

    08/29/2019

    The growing number of RF, microwave, and millimeter-wave applications has led to a growth in the number of RF transistor types, semiconductors, and configurations being used today. As more devices use RF/wireless technology to communicate and sense, there will be an even greater diversity of RF transistor technologies. RF Amplifiers and RF Mixers are a ..

    Read Full Article

    What are Metamaterials and How Do They Relate to Antennas?

    08/22/2019

    Metamaterials are an increasingly researched topic, especially where it pertains to modern antenna structures. However, there is a lot of confusion of exactly what metamaterials are and how they are involved in the development of antennas. To put it simply, metamaterials are material and structure combinations that exhibit properties that are otherwise unknown to occur ..

    Read Full Article
    Jump to of 37
    Live help