Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • Millimeter-wave Interconnect Considerations

    08/26/2021

    There has been a general trend of radio and sensing applications shifting to higher frequencies, either to avoid interference due to the growing use of RF and microwave spectrum or to take advantage of the growing accessibility of millimeter-wave hardware. This is true for consumer, industrial, military, aerospace, and satellite communications applications alike. Regardless of ..

    Read Full Article

    MIMO vs SISO – Antenna Technology

    08/12/2021

    Though the terms single-input single-output (SISO) and multi-input multi-output (MIMO) originate with controls engineering, SISO and MIMO are now very commonly discussed in reference to RF antennas. In controls engineering, a SISO system has only one input and one output, such as a DUT with only 2-ports that you can measure with a 2-port Vector ..

    Read Full Article

    Waveguide Horn Antenna Primer

    07/29/2021

    A waveguide horn antenna is a type of aperture antenna that is designed with a gradual transition of the inner metallic walls to ensure an impedance match between the waveguide port to free space. In this way, a waveguide horn antenna’s aperture and axial length can be adjusted to achieve the desired gain and directivity ..

    Read Full Article

    Indium Phosphide (InP) versus GaAs for Gunn Diode Oscillators

    07/15/2021

    Gunn Diodes have been used to build upper microwave, millimeter-wave, and even terahertz oscillators for a wide range of applications over 40 years. To this day, Gunn Diode oscillators are competitive with monolithic microwave integrated circuit (MMIC) oscillator solutions. Hence, Gunn Diodes have been the premier solid-state coherent power generation device at frequencies above ~10 ..

    Read Full Article

    Advantages of the Double Ridge Waveguide Design

    07/01/2021

    Waveguides come in many varieties. The most common “shapes” for waveguide cross sections are rectangular and circular/oval. Waveguide can carry electromagnetic energy in several modes, though they are typically specified for a primary mode that presents the most desirable characteristics for loss and bandwidth. This mode is generally the transverse electric (TE) mode, where the ..

    Read Full Article

    RF Component & Device Test Series: RF Filter Testing

    06/17/2021

    RF Frequency filters, or just filters, are components/devices that modify a signal’s amplitude and phase angle based on frequency. Filters are either passive or use active tuning electronics. Filters are designed with a predetermined frequency dependent transmission response and are predominately used to attenuate portions of the spectrum where undesirable signal components, interference, or noise ..

    Read Full Article

    RF Component & Device Test Series: RF Low Noise Amplifier Testing

    06/03/2021

    Low noise amplifiers (LNAs) are a critical component for telecommunication and sensing systems, as the weak receive signals often need to be at a higher signal level for optimal demodulation, digitization, driving another circuit, or for measurements to be made. LNAs are also used throughout signal chains to add gain to low power signals when ..

    Read Full Article

    RF Component & Device Test Series: How Are Active RF Devices Tested

    05/20/2021

    RF devices are active elements in the RF signal chain and are used in almost all RF systems with exception of purely passive systems. Active RF devices are distinguished from passive RF devices in that electrical power or electrical control signals are used to energize the device and change its performance. In many cases, active ..

    Read Full Article

    RF Component & Device Test Series: How Are RF Passive Devices Tested

    05/13/2021

    RF passive components are used in virtually every RF assembly and system for communications, sensing, and test and measurement applications. Hence, testing RF passives is critical to all applications. RF passives testing may be for characterization, quality control/verification, or maintenance/troubleshooting depending on the use case of the RF passive and if it is under development, ..

    Read Full Article

    Microwave Measurement Methods of Dielectrics

    05/06/2021

    Conductors, semiconductors, and insulators are the main building blocks of virtually all RF/microwave electronics. Insulators have dielectric properties that impact the electric fields that pass through them. In order to design an RF component or device, detailed knowledge of the dielectric properties of the insulators used in the construction of the component/device is essential. The ..

    Read Full Article
    Jump to of 38
    Live help