Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • Coaxial Cable Assemblies for Rugged Outdoor Applications

    12/15/2022

    RF Coaxial Cable Assemblies are used in virtually all environments where wireless systems are deployed. Coaxial cable assemblies are integral internal parts of many wireless systems, and they are also used as interconnects between systems. These cable assemblies are often anywhere from a few inches long to hundreds of feet in length. This range of ..

    Read Full Article

    Power Added Efficiency (PAE) Calculator Explained

    12/01/2022

    RF power amplifiers typically have an input, output, and power supply rails. These rails can be either positive, negative, or dual positive and negative voltages. The input, output, and power supply rails all have recommended operating ranges of power, voltage, and current. This range is specified to nominal operation in what the manufacturer was able, ..

    Read Full Article

    Pasternack’s 50th Anniversary! An Interview with the Man who Started it all

    11/14/2022

    Pasternack has a milestone anniversary this year! Fifty years later, Pasternack products are as relevant and renowned as ever, and there’s no slowing down. To celebrate this momentous occasion, we recently had the opportunity take a trip down memory lane and learn the history of the brand from Murray Pasternack, the founder of Pasternack. Read ..

    Read Full Article

    Coaxial Cable Impedance Calculator

    11/03/2022

    The dominant use of coaxial cable in RF & Microwave applications is as a transmission line. Coaxial cables are extremely useful transmission lines as the coaxial nature of the transmission line provides relatively efficient transmission from DC to a cut-off frequency, which is a function of the geometries of the coaxial components of the cable. ..

    Read Full Article

    Antenna Downtilt & Coverage Calculator Chart

    10/20/2022

    An Antenna Downtilt and Coverage Calculator, or Antenna Tilt Calculator, aids the user by providing an approximate downward angle at which to install a directional antenna to reach desired signal strength and coverage between a transmitter and receiver at different heights and some distance away. An example use case is when a cell-tower directional transceiver ..

    Read Full Article

    VSWR, Return Loss, Insertion/Transmission loss vs. Transmission Power

    09/22/2022

    In an ideal RF system, all of the energy from the RF source is transferred to the load. An example of this would be a transmitter delivering a signal to an antenna with the interconnect between the two signal chain components operating at 100% efficiency. Clearly, this isn’t the case, and factors like impedance mismatch ..

    Read Full Article

    Instant C to F Calculator: Convert Celsius to Fahrenheit in Seconds

    09/17/2022

    When it comes to temperature conversions, switching between Celsius and Fahrenheit can be confusing. Whether you’re traveling, cooking, or working on science projects, knowing how to convert Celsius to Fahrenheit (or vice versa) is crucial. That’s where an instant C to F calculator comes in handy. In this article, we’ll walk you through everything you ..

    Read Full Article

    All About RF Coaxial Connectors

    09/08/2022

      RF coaxial connectors are one of the most useful and ubiquitous methods of connecting RF systems and components. RF coaxial connectors are coaxial transmission lines made up of an RF coaxial cable and RF coaxial connectors terminating either end of the cable. RF connectors provide interconnect with other RF connectors, which must be of ..

    Read Full Article

    How to Use the Cable Creator Tool

    08/25/2022

    The Pasternack The Cable Creator Tool™ is a powerful method of ordering custom coaxial cable, where all cable assemblies ordered through the tool are typically built and shipped the same day as ordered. The selection of connector types, cable types, and configurations are extremely diverse and should fill virtually any coaxial cable assembly need. The ..

    Read Full Article

    Why Hermetically Seal RF Adapters and how is it done?

    08/11/2022

    RF coaxial adapters are often the difference between expensive options of reordering RF cable assemblies, RF connectors, or even retrofitting RF assemblies with new RF coaxial connectors, and a few seconds of installing a quick fix. Also, RF adapters are useful in protecting/extending the life of the RF ports of expensive to service and replace ..

    Read Full Article
    Jump to of 38
    Live help