Pasternack Blog

  • Categories

  • Archive

  • Signal Chain Discussion Series: Difference Between IF & RF

    12/10/2020

    In many cases in RF/Microwave electronics it is advantageous to generate, modulate, receive, and demodulate communication and sensing signals at frequencies lower than the RF transmission/reception carrier frequency. The frequency difference between the modulation/demodulation (baseband) signals and the RF signals may be so vast, that multiple frequency conversion stages may be required. In these instances, ..

    Read Full Article

    Signal Chain Discussion Series: Transmit/Receive Module

    11/12/2020

    Though transmit/receive modules (TRMs) have been used for some time in active electronically scanned array (AESA) radar technology, the benefits of phased array antenna and multi-input-multi-output (MIMO) for 5G applications have brought this technology to the mainstream. Given that phase array antennas for millimeter-wave 5G may employ up to, and possibly beyond, 64 antennas elements ..

    Read Full Article

    Signal Chain Discussion Series: Communications Transceiver

    10/29/2020

    A communications transceiver performs the task of converting digital or analog signals to RF, transmitting those signals, and receiving incoming signals for conversion back to digital or analog signals. Hence, the key components of a communications transceiver are the modulation/demodulation circuitry, transmitter, and receiver. Depending on the architecture of the communications transceivers, direct digital synthesizers ..

    Read Full Article

    Purpose of Positive Gain Slopped Equalizers

    10/01/2020

    In wide-band microwave systems there is a tendency for the gain to roll-off at higher frequencies, reducing the overall gain-flatness of the system due to the negative gain slope of signal chain components. Active devices, such as amplifiers tend to exhibit a negative gain slope, as well as passive components, such as connectors, adapters, coaxial ..

    Read Full Article

    Brief on Frequency Dependent Conductivity In Metallic Wires/Traces

    09/03/2020

    It has been understood for nearly a century that the conductivity of conductive metals changes as a function of frequency. Though this is the case the phenomenon behind frequency dependent conductivity is not as well understood by man. It was observed early on that the attenuation and resistive losses of metallic transmission lines and traces ..

    Read Full Article

    Why Hermetic Enclosures/Sealing?

    08/27/2020

    A hermetically sealed enclosure, or hermetic packaging, is a method of encapsulating a device or system in an environmentally protected package that prevents the exchange of the inside and outside environment. Hermetic packages are commonly seen in automotive, industrial, naval, military, and aerospace applications where the outside environment may lead to damage, early failure, or ..

    Read Full Article

    Harping on Harmonics

    08/20/2020

    Harmonics are spurious signal content (or spurious emissions) that are generated by a single frequency tone and nonlinear elements within a RF/microwave signal chain, or single-tone intermodulation distortion (IMD). The nonlinear elements create harmonics that are integer multiples of the fundamental frequency (often called the first harmonic). For instance, fo is the fundamental frequency and ..

    Read Full Article

    What Are Dynamic Range, SNR, P1dB, and Other Common RF/Microwave Characteristics

    08/13/2020

    There are several key methods of describing RF signal quality and device performance in respect to noise and linearity. As noise and linearity are often key considerations of both transmit and receive chains in communications and sensing systems, it is valuable for a technical professional to understand these parameters. The same fundamentals that govern radar ..

    Read Full Article

    High Power RF/Microwave Considerations

    07/30/2020

    Like with other key RF/microwave component and device parameters, accounting for power extremes in RF design and system integration requires a nontrivial amount of additional considerations. If the RF signal is optimized for other performance factors, such as noise, linearity, phase noise, or other signal quality factors and the signal power is well within the ..

    Read Full Article

    Basics of Satellite Ground Station Hardware

    07/23/2020

    A ground station, earth station, or earth terminal is the terrestrial radio system used in extraplanetary telecommunications with spacecraft and satellites. Ground stations are used to communicate, bidirectionally, with satellites and spacecraft, or receive electromagnetic energy in the radio frequency spectrum from astronomical sources. Given the nature of extraplanetary communications, ground stations and satellites/spacecraft typically ..

    Read Full Article
    Jump to of 8