Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • Microwave Measurement Methods of Dielectrics

    05/06/2021

    Conductors, semiconductors, and insulators are the main building blocks of virtually all RF/microwave electronics. Insulators have dielectric properties that impact the electric fields that pass through them. In order to design an RF component or device, detailed knowledge of the dielectric properties of the insulators used in the construction of the component/device is essential. The ..

    Read Full Article

    Updates on RF Silicon Technology

    03/18/2021

    Though Gallium Nitride (GaN) has been making headlines for the past several years as an emerging RF technology, RF semiconductors developed with silicon, namely RF silicon-on-insulator (RF-SOI), has also been advancing as a semiconductor of choice for the exploding RF hardware markets.  Where GaN is a still relatively expensive and small wafer technology, RF-SOI is ..

    Read Full Article

    Overview of Ferrite-based RF Technology

    01/28/2021

    Ferrites are high electrical resistance, magnetic, and ceramic materials constructed from a mix of metallic oxides, often including Iron (Fe), Zinc (Zn), Manganese (Mn), Nickel (Ni), Cobalt (Co), Barium (Ba), and Strontium (Sr). These metallic oxides exhibit magnetic behavior that allows for their use in RF circuits as inductors, transformers/baluns, isolators, circulators, phase shifters, chokes, ..

    Read Full Article

    Signal Chain Discussion Series: Difference Between IF & RF

    12/10/2020

    In many cases in RF/Microwave electronics it is advantageous to generate, modulate, receive, and demodulate communication and sensing signals at frequencies lower than the RF transmission/reception carrier frequency. The frequency difference between the modulation/demodulation (baseband) signals and the RF signals may be so vast, that multiple frequency conversion stages may be required. In these instances, ..

    Read Full Article

    Signal Chain Discussion Series: Transmit/Receive Module

    11/12/2020

    Though transmit/receive modules (TRMs) have been used for some time in active electronically scanned array (AESA) radar technology, the benefits of phased array antenna and multi-input-multi-output (MIMO) for 5G applications have brought this technology to the mainstream. Given that phase array antennas for millimeter-wave 5G may employ up to, and possibly beyond, 64 antennas elements ..

    Read Full Article

    Signal Chain Discussion Series: Communications Transceiver

    10/29/2020

    A communications transceiver performs the task of converting digital or analog signals to RF, transmitting those signals, and receiving incoming signals for conversion back to digital or analog signals. Hence, the key components of a communications transceiver are the modulation/demodulation circuitry, transmitter, and receiver. Depending on the architecture of the communications transceivers, direct digital synthesizers ..

    Read Full Article

    Purpose of Positive Gain Slopped Equalizers

    10/01/2020

    In wide-band microwave systems there is a tendency for the gain to roll-off at higher frequencies, reducing the overall gain-flatness of the system due to the negative gain slope of signal chain components. Active devices, such as amplifiers tend to exhibit a negative gain slope, as well as passive components, such as connectors, adapters, coaxial ..

    Read Full Article

    Brief on Frequency Dependent Conductivity In Metallic Wires/Traces

    09/03/2020

    It has been understood for nearly a century that the conductivity of conductive metals changes as a function of frequency. Though this is the case the phenomenon behind frequency dependent conductivity is not as well understood by man. It was observed early on that the attenuation and resistive losses of metallic transmission lines and traces ..

    Read Full Article

    Why Hermetic Enclosures/Sealing?

    08/27/2020

    A hermetically sealed enclosure, or hermetic packaging, is a method of encapsulating a device or system in an environmentally protected package that prevents the exchange of the inside and outside environment. Hermetic packages are commonly seen in automotive, industrial, naval, military, and aerospace applications where the outside environment may lead to damage, early failure, or ..

    Read Full Article

    Harping on Harmonics

    08/20/2020

    Harmonics are spurious signal content (or spurious emissions) that are generated by a single frequency tone and nonlinear elements within a RF/microwave signal chain, or single-tone intermodulation distortion (IMD). The nonlinear elements create harmonics that are integer multiples of the fundamental frequency (often called the first harmonic). For instance, fo is the fundamental frequency and ..

    Read Full Article
    Jump to of 8
    Live help