Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • Ensuring Reliability in Space-Grade RF Coaxial Interconnects

    05/30/2025

    In the unforgiving environment of space, RF coaxial interconnects must meet rigorous demands for performance, durability, and consistency. From extreme temperature fluctuations to high levels of radiation and vibration, these components are essential to mission success. In our latest article for Microwave Journal, Pasternack explores the essential design and material considerations for building space-grade RF ..

    Read Full Article

    What Are Coaxial Connector Adapters?

    02/16/2023

    RF Coaxial Connector Adapters are simply RF Coaxial Connectors with a common internal transmission line and specific coaxial connector types or genders on either end. For instance, some RF Adapters are simply coaxial connector male-to-male or female-to-female adapters, which allows for the interconnection of a male coaxial connector to another male coaxial connector or a ..

    Read Full Article

    How are End-launch, PCB Connectors Useful?

    05/21/2020

    There has been an increasing use of RF coaxial connectors, especially microwave and millimeter-wave coaxial connectors, for high-speed digital and precision sensing applications, There are also a growing trend toward highly compact and interconnect dense microwave and millimeter-wave systems, such as multi-input multi-output (MIMO) antennas for 5G and actively electronically scanned array (AESA) radar antennas. ..

    Read Full Article

    Round-up of RF Quick Connect/Quick Disconnect Connectors

    12/13/2018

    From Threaded to Quick The technology for RF threaded connectors began in the early days of UHF communications and, since that time, other RF connectors have been developed to meet the needs of advancing technologies in the communications industry. In the early 1990’s, RF manufactures needed RF cable assemblies with interconnects that could manage the ..

    Read Full Article

    Upper Microwave and Millimeter-wave Frequency Coaxial Connector Overview

    10/18/2018

    Many coaxial connector types are available in the RF and microwave industry designed for specific purposes and applications with smaller connectors that perform into the GHz and millimeter wave range. Compatibility with other RF microwave components is achieved with universally accepted connector standards so that interconnecting coaxial modules within a system is possible and must ..

    Read Full Article

    BMA Connectors Push beyond Twist Tighten RF Connectors

    04/12/2018

    In many applications, a threaded RF connection may be impractical, or even impossible. Some examples include panel, daughter cards, or inserts with many RF connections. In these cases the pitch between the connectors may necessarily be too small for a threaded nut, or the card/assembly may be inserted into a slot where there is no ..

    Read Full Article

    What is so Special About the 4.3-10 Coaxial Connector?

    04/05/2018

    There are many coaxial connectors used in wireless and wired networks, including DIN 7/16, N, 4.1/9.5, and the 4.3-10 interface. Typically, the choice of a connector boils down to economics, power handling, size, and installation criteria. However, the increasing number of wireless network bands and mobile data rates pose a very stringent requirement for transmission ..

    Read Full Article

    What you need to know about Reverse Polarized Connectors

    04/20/2017

    A reverse polarized coax connector is a variation of a standard polarity connector in which the gender of the interface has been reversed. The term “reverse polarity” refers not to the signal polarity of the connector itself but to the gender of the center contact pin. A reverse polarized connector will have the same external ..

    Read Full Article
    Jump to of 1
    Live help