Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • What Is A RF Amplifier, And What Are They Used For?

    10/17/2024

    Within an RF signal chain, there is often the need to provide some signal conditioning in incoming, outgoing, or through signals. One of the most needed signal conditioning methods is amplification of signal energy, which is the key function of RF Amplifiers. Signal amplification involves increasing the amplitude of a signal, this could imply voltage, ..

    Read Full Article

    RF Low Noise Amplifiers (LNAs) Applications & Considerations

    10/03/2024

    Throughout the signal chain and especially at a signal input stage, RF signals for communications and sensing can be extremely weak. RF Low Noise Amplifiers (LNAs) are the most common method for increasing the signal level of these very weak signals while minimizing the introduction of signal degrading factors. Of these signal degrading factors, added ..

    Read Full Article

    What Is High Gain and How Does It Impact Amplifier Performance?

    09/19/2024

    RF sensing and communication applications often involve very weak signal levels. It is often necessary to use RF Amplifiers to increase the gain, or signal level, of these signals in order to digitize them or otherwise condition these signals to usable levels. However, there are a few trade-offs to consider when increasing a signal’s power ..

    Read Full Article

    Harnessing the Potential of the 110 MHz Frequency with Broadband Amplifiers

    02/27/2024

    Whether used in communication networks, broadcasting systems, or advanced testing environments, the 110 MHz frequency requires precision tools to amplify signals and minimize interference. In communication networks, broadcasting systems, or advanced testing environments, this frequency requires precision tools to amplify signals and minimize interference. Tools like 110 MHz frequency broadband amplifiers ensure seamless signal transmission ..

    Read Full Article

    The Difference between RF Amplifier Types

    08/04/2022

    At first look, there are many different types of RF amplifiers, and it could be overwhelming to go from the specs you need to narrowing down what RF amplifier type is the best fit. Most RF amplifier types came about from the specification requirements of common transceiver, receiver, transmitter, radar, and modulation circuits and system-level ..

    Read Full Article

    Bidirectional Amplifier Basics

    06/23/2022

    A Bidirectional Amplifier, or Bi-directional Amplifier (bda), is an active RF device that is widely used in a variety of telecommunication, radar, and other RF sensing applications. Though conceptually a Bidirectional Amplifier performs a relatively simple operation, the internal electronics can be somewhat complex. Moreover, many applications favor certain names and types of Bidirectional Amplifiers, ..

    Read Full Article

    What Makes a Hi-Rel Amplifier Hi-Rel?

    09/23/2021

    The main application for High Reliability (Hi-Rel) RF/microwave amplifiers is for military, defense, aerospace, and other critical applications where device reliability is otherwise mission critical. In essence, a Hi-Rel Amplifier is just an amplifier that meets one or more military standards for reliability. In order to ensure device and system reliability, the US military developed ..

    Read Full Article

    Waveguide Amplifier Introduction & Applications

    04/29/2021

    Waveguide amplifiers are amplifiers specifically designed to be housed within a waveguide assembly. This provides some intrinsic advantages and trade-offs compared with coaxial connectorized amplifier assemblies or pallet amplifiers. Given that waveguide amplifiers are designed to directly mate with a given waveguide size and type, they are innately banded, as the waveguide has a limited ..

    Read Full Article

    New Applications for Bi-Directional Amplifiers – Unmanned Systems

    01/07/2021

    In a similar way to how wireless technology is enabling new functionality and opportunities in civilian life, there are a wealth of military applications embracing, and being enhanced, by wireless technology. Unlike civilians, military operators require a much higher level of reliability and redundancy, as a few second gap in coverage for a military operator ..

    Read Full Article

    Waveguide Amplifier Introduction & Applications

    05/14/2020

    Waveguide amplifiers, or full-band/multi-band waveguide amplifiers, are amplifiers housed in assemblies that have either waveguide or coaxial interconnect. Though waveguide interconnect is more common for waveguide amplifiers, some waveguide amplifiers have coaxial interconnect instead, but still perform as specified over a given waveguide frequency band. The main feature of waveguide amplifiers is that they are ..

    Read Full Article
    Jump to of 2
    Live help