Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • Introduction to MIL-PRF-39012 and MIL-STD-348 Coaxial Connectors

    02/02/2026

    To enable interoperability amongst RF systems, the military and industry rely on standardized dimensions and types of coaxial connectors. The two major standards that define coaxial connectors for the US military are MIL-STD-348 and MIL-PRF-39012. MIL-STD-348 provides the dimensions for control of the standard interfaces, while MIL-PRF-39012 defines the, detail specifications, materials, quality conformance, qualification, ..

    Read Full Article

    Coaxial Connector Adapter Dynamics

    06/27/2024

    The number and type of coaxial connector standards, both open and proprietary, is steadily growing. The growth and diversity of coaxial connector standards is partly fueled by the growing diversity of wireless applications and the penetration of RF technologies in virtually every market. This is why Coaxial connector adapters, a subset of RF adapters, are ..

    Read Full Article

    NEX10 Cable Assemblies Features and Applications

    06/13/2024

    Developed specifically for small cell applications, the NEX10 connector system is a new connector interface that exhibits low-PIM, excellent return loss, and other features desirable for high speed RF communication installations. With the rise of higher frequency bands used in cellular, Wi-Fi, and other communications applications, there has been an opportunity for a small and ..

    Read Full Article

    Subminiature Version B (SMB) Coaxial Connectors

    04/18/2024

    Subminiature Version B (SMB) Connectors are a coaxial connector type that has been around for roughly 60 years. SMB connectors are among the snap-on, blind-mate, or push-connect type of coaxial connectors and can be found as either 50 Ohm or 75 Ohm varieties. These connectors are generally specified to operate from DC to 2 GHz, ..

    Read Full Article

    All About D-Sub Connectors

    04/04/2024

    D- Subminiature connectors, or D-Sub connectors, are a compact and versatile connector platform that can support power, analog, RF, or digital signal transmission. Depending on the type of D-Sub Connectors used, a D-Sub connector could support connections from every domain, which makes these an extremely common connector interface for a wide range of applications. These ..

    Read Full Article

    Why 2.4mm Connectors Are the Backbone of High-Frequency, Eco-Compliant RF Systems

    11/05/2023

    In the world of RF and microwave engineering, 2.4mm connectors are indispensable, particularly in high-frequency and precision applications. Designed with a focus on handling high-frequency signal applications, these RF connectors are key to industries that require low-loss signal integrity and robust connectivity, such as telecommunications, aerospace, and advanced research labs. Because they also satisfy stringent ..

    Read Full Article

    Deciphering TRB, TRT, TRS, TTM, TRC, TRN, TWBNC, TWTNC, Triax, Twinax, and other coaxial and triaxial connector terms

    09/28/2023

    As is common in many industries, there are often internal acronyms or company part names/standards that may eventually spread to the larger industry. This is the case for some of the types of twinaxial and triaxial transmission line components, such as TRB Plug to TRB Jack Right Angle Adapters, that are present in the RF ..

    Read Full Article

    All About 7/16 DIN Connectors

    03/16/2023

    7/16 DIN Connectors, or DIN 7/16 connectors, are one of the most common coaxial connector types used for interconnect between cellular networking systems and cellular antennas. 7/16 DIN connectors are 50 Ohm connectors with relatively high-power handling and exceptional passive intermodulation distortion performance. The high-power handling capability of this connector type compared to N connectors ..

    Read Full Article

    3.5 mm Coaxial Cable Adapters Overview

    03/02/2023

    The 3.5 mm Coaxial Connector is a widely used standardized coaxial connector type with some interesting features. These features make the 3.5 mm Coaxial Connector a very common connector type, which is why there are a plethora of 3.5 mm Coaxial Adapters. The 3.5 mm Coaxial Connector is designed to be relatively rugged and uses ..

    Read Full Article

    SMA Connector Overview

    12/29/2022

    SMA Coaxial Connectors, or just SMAs, are one of the most common coaxial connector types used throughout the RF, microwave, and even millimeter-wave (mmW) industries. SMA stands for subminiature version A and was developed in the 1960s. The interface dimensions and other aspects of the SMA connector are detailed in MIL-STD-348 and was originally designed ..

    Read Full Article
    Jump to of 2
    Live help