Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • Everything You Need to Know About the RG 6 Crimping Tool

    10/11/2021

    When it comes to installing or repairing coaxial cables, one of the most important tools is the RG 6 crimping tool. The RG 6 crimping tool is a specialized tool designed to create strong, secure connections between RG 6 coaxial cables and their connectors.  Whether you’re a seasoned professional or new to repair and installs, ..

    Read Full Article

    Uses for Matching Pads

    10/07/2021

    The terms Impedance Matching Pads, resistive impedance transformers, or minimum loss pads all refer to the same RF components that solve a relatively common problem in some applications that have equipment, components, and devices at different standard impedances. For example, many broadcast, TV, and military communication systems use 75 ohms as a standard characteristic impedance, ..

    Read Full Article

    Understanding the 2.92mm Connector

    09/24/2021

    In the realm of high-frequency signal transmission, the choice of connectors is crucial for maintaining signal integrity and overall system performance. One connector that stands out for applications up to 40 GHz is the 2.92mm connector, commonly known as the K connector. This blog post delves into what the 2.92mm connector is, where it’s used, ..

    Read Full Article

    What Makes a Hi-Rel Amplifier Hi-Rel?

    09/23/2021

    The main application for High Reliability (Hi-Rel) RF/microwave amplifiers is for military, defense, aerospace, and other critical applications where device reliability is otherwise mission critical. In essence, a Hi-Rel Amplifier is just an amplifier that meets one or more military standards for reliability. In order to ensure device and system reliability, the US military developed ..

    Read Full Article

    Understanding Micro wave Antennas: What They Are and How They’re Used

    09/18/2021

    In today’s world of fast-paced communication, micro wave antennas play a crucial role in microwave communication systems. These antennas are essential for transmitting and receiving electromagnetic waves at microwave frequencies, typically ranging from 1 GHz to 100 GHz. In this blog post, we’ll dive into what micro wave antennas are, how they work, and explore ..

    Read Full Article

    All About Waveguide Shorts and Shims

    09/09/2021

    For many RF test applications in the higher frequencies, such as millimeter-waves, or for high power use cases, rectangular waveguides are the interconnect solution of choice. In a similar wave to short-open-load-through (SOLT) calibration standards used for vector network analyzer (VNA) calibration with coaxial interconnect, VNA using waveguide interconnect requires waveguide calibration standards. Even with ..

    Read Full Article

    Millimeter-wave Interconnect Considerations

    08/26/2021

    There has been a general trend of radio and sensing applications shifting to higher frequencies, either to avoid interference due to the growing use of RF and microwave spectrum or to take advantage of the growing accessibility of millimeter-wave hardware. This is true for consumer, industrial, military, aerospace, and satellite communications applications alike. Regardless of ..

    Read Full Article

    MIMO vs SISO – Antenna Technology

    08/12/2021

    Though the terms single-input single-output (SISO) and multi-input multi-output (MIMO) originate with controls engineering, SISO and MIMO are now very commonly discussed in reference to RF antennas. In controls engineering, a SISO system has only one input and one output, such as a DUT with only 2-ports that you can measure with a 2-port Vector ..

    Read Full Article

    Waveguide Horn Antenna Primer

    07/29/2021

    A waveguide horn antenna is a type of aperture antenna that is designed with a gradual transition of the inner metallic walls to ensure an impedance match between the waveguide port to free space. In this way, a waveguide horn antenna’s aperture and axial length can be adjusted to achieve the desired gain and directivity ..

    Read Full Article

    Indium Phosphide (InP) versus GaAs for Gunn Diode Oscillators

    07/15/2021

    Gunn Diodes have been used to build upper microwave, millimeter-wave, and even terahertz oscillators for a wide range of applications over 40 years. To this day, Gunn Diode oscillators are competitive with monolithic microwave integrated circuit (MMIC) oscillator solutions. Hence, Gunn Diodes have been the premier solid-state coherent power generation device at frequencies above ~10 ..

    Read Full Article
    Jump to of 31
    Live help