Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • Subminiature Version B (SMB) Coaxial Connectors

    04/18/2024

    Subminiature Version B (SMB) Connectors are a coaxial connector type that has been around for roughly 60 years. SMB connectors are among the snap-on, blind-mate, or push-connect type of coaxial connectors and can be found as either 50 Ohm or 75 Ohm varieties. These connectors are generally specified to operate from DC to 2 GHz, ..

    Read Full Article

    3.5mm Adapter use in RF Applications for 50 Ohm Systems

    04/09/2024

    The 3.5mm adapter is a crucial component in RF applications, particularly in 50-ohm systems, where signal integrity and performance are of utmost importance. These adapters are known for their precision and high-frequency capability, making them a popular choice for industries relying on reliable RF connections. The versatility and durability of the 3.5mm adapter make it ..

    Read Full Article

    All About D-Sub Connectors

    04/04/2024

    D- Subminiature connectors, or D-Sub connectors, are a compact and versatile connector platform that can support power, analog, RF, or digital signal transmission. Depending on the type of D-Sub Connectors used, a D-Sub connector could support connections from every domain, which makes these an extremely common connector interface for a wide range of applications. These ..

    Read Full Article

    What is Pasternack’s Custom-To-Standard Initiative & How Does This Benefit Coaxial Cable Buyers

    03/21/2024

    The number and type of RF, microwave, and millimeter-wave applications are growing at an explosive rate. Every year new product types, wireless protocols, end-uses, and equipment to help test and fabricate these new technologies emerge. Coaxial cables are one of the most commonly used interconnect types that pervades virtually every RF application. This is why ..

    Read Full Article

    Understanding 3.5mm Cable in RF Applications for 50 Ohm Systems

    03/09/2024

    In the world of radio frequency (RF) systems, reliable and precise signal transmission is critical. One of the essential components used in these systems is the 3.5mm cable. Known for its durability and high-frequency performance, the 3.5mm cable is frequently employed in 50-ohm RF applications where performance and impedance matching are crucial to the overall ..

    Read Full Article

    What Are Standard Gain Horn Antennas & Accessories Used For?

    03/07/2024

    A standard gain horn antenna is a type of waveguide antenna that is used in a variety of test/measurement, sensing, radar, and communications applications. Waveguide antennas, such as standard gain horns are used in these applications due to their high gain, efficiency, and precision performance. There are Standard Gain Horn Antennas With Waveguide Input and ..

    Read Full Article

    Harnessing the Potential of the 110 MHz Frequency with Broadband Amplifiers

    02/27/2024

    Whether used in communication networks, broadcasting systems, or advanced testing environments, the 110 MHz frequency requires precision tools to amplify signals and minimize interference. In communication networks, broadcasting systems, or advanced testing environments, this frequency requires precision tools to amplify signals and minimize interference. Tools like 110 MHz frequency broadband amplifiers ensure seamless signal transmission ..

    Read Full Article

    Demystifying Low Loss Coaxial Cable Terms

    02/22/2024

    When looking into coaxial cable for a variety of applications, from commercial wireless to audio/visual broadcast, it is not uncommon to come across coaxial cable types labeled as LMR-, CFD-, OFC-, etc. at several different indicators, such as 195, 200, 240, 400, or 600. An example of this is Low Loss Flexible LMR-400 Plenum Rated ..

    Read Full Article

    How to Calculate Frequency from Wavelength

    02/15/2024

    The concept of calculating frequency from wavelength is fundamental in the study of waves, including electromagnetic waves like light and radio. Understanding how these two properties relate, and how to calculate frequency from wavelength, can be useful in fields like telecommunications, physics, and engineering. Whether you’re working with sound waves, microwaves, or visible light, being ..

    Read Full Article

    What Is A 2.4 GHz Antenna?

    01/25/2024

    There is a plethora of wireless communications antennas labeled as a 2.4 GHz antenna, this does not mean that these antennas only operate at exactly 2.4 GHz. It implies that they cover some area of the 2.4 GHz ISM band, which extends from 2.4 GHz to 2.5 GHz. In most cases, for the 2.4 GHz ..

    Read Full Article
    Jump to of 31
    Live help