Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • The Difference between MIL-STD, MIL-HDBK, MIL-DTL, MIL-PRF and MIL-SPEC

    05/18/2017

    The US defense standards, commonly referred to as MilSpec, are developed by the US DoD for the purpose of enhancing interoperability among critical defense systems. The goal of the standards is to provide precise descriptions on the procedures and practices for the design, manufacturing, and deployment of military devices and equipment. Ultimately, the standards aim ..

    Read Full Article

    Waveguides Inside Out

    05/11/2017

    Following from the name, a waveguide is a hollow conductive structure that guides an EM wave along a path. The conductive inner walls of the waveguide bounce EM energy along the path with low-loss and close to light speed. Waveguides are commonly cylindrical, elliptical, or rectangular. In a rectangular waveguide, transverse electric (TE), or H-wave, ..

    Read Full Article

    When and Where You Need RF Limiters and Detectors

    05/04/2017

    RF limiters and detectors are used widely throughout the RF and microwave industry in a wealth of circuit applications. For example, radar transceivers, telecommunication radios, test and measurement equipment, and other circuits rely on RF limiters for receiver protection, as well as the protection of critical circuit components that may experience high-peak voltage and current ..

    Read Full Article

    What is Passive Intermodulation (PIM) Distortion, and how can it be Mitigated?

    04/27/2017

    Passive intermodulation (PIM) distortion is a wireless communication system degrading phenomenon that has been a concern for cellular telecommunications, satellite communications, and wireless network development. PIM is such a concern in cellular/wireless communications that there are entire distinct Low PIM Components and Cable Assemblies product lines designed to aid in preventing or mitigating PIM distortion. ..

    Read Full Article

    What you need to know about Reverse Polarized Connectors

    04/20/2017

    A reverse polarized coax connector is a variation of a standard polarity connector in which the gender of the interface has been reversed. The term “reverse polarity” refers not to the signal polarity of the connector itself but to the gender of the center contact pin. A reverse polarized connector will have the same external ..

    Read Full Article

    What do RoHS, REACH, and WEEE Mean for RF/Microwave Components, Manufacturers and Assemblers?

    04/13/2017

    RoHS, also known as Lead-Free, stands for Restriction of Hazardous Substances. RoHS originated in the European Union and restricts the use of six hazardous materials found in electrical and electronic products. All applicable products in the EU market after July 1, 2006 must pass RoHS compliance. The substances banned under RoHS are lead (Pb), mercury ..

    Read Full Article

    RF Amplifier Packaging and Thermal Dynamics

    04/06/2017

    Packaging dimensions, weight, pinouts and material construction are critical features of any RF amplifier. These factors heavily weigh into the cost and feasibility of using a particular amplifier in a given design. Regardless of electrical and RF performance, if an amplifier can’t fit into the required footprint, the device won’t be serviceable for that application. ..

    Read Full Article

    Cheap Waveguides can Ruin your Day

    03/30/2017

    Though there are many reputable and high quality waveguide vendors, some vendors, specifically offshore vendors, may use machining techniques that reduce time and cost of manufacture. These short-cuts could have dramatic impact on a waveguide component and system performance. Any misalignments or machined geometries beyond specified levels can reduce the VSWR performance of a waveguide, ..

    Read Full Article

    Practical Mixers 101

    03/23/2017

    Introduction to Mixers A microwave frequency mixer is a 3-port electronic circuit that combines two or more signals into one or two composite output signals, and are categorized as switching mixers or nonlinear mixers– although many mixers are configured with both. Using diodes, the mixer is passive and has a conversion loss. Using active devices, ..

    Read Full Article

    RF and Microwave Attenuator Fundamentals

    03/16/2017

    RF attenuators are fundamental components of RF and Microwave circuits and systems. Often found in virtually every RF application, attenuators play a vital role in receivers, transmitters, test and measurement systems etc. The main purpose of attenuators is to reduce the signal strength, such as prior to the signal reaching a sensitive circuit element. Attenuators ..

    Read Full Article
    Jump to of 31
    Live help