Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • Distributed Antenna System (DAS) Basics

    03/29/2018

    There are many cases, especially within buildings, tunnels, large public venues, stadiums, and etc. where the signals from a cell tower does not provide sufficient coverage, or the density of users is just too great for a typical cellular approach. In these circumstances DAS installation can be employed to enhance the coverage in these areas, ..

    Read Full Article

    Small Cells are Certainly Making a Large Impact

    03/15/2018

    Small Cells are essentially a mobile wireless installation that is smaller in scope and size than a traditional macro base station. So, why are Small Cells, which provide less coverage and necessarily are composed of equipment that may not have the full capability of macro-cells, on the rise? An important note is that the term ..

    Read Full Article

    The 5th Generation of Mobile Wireless (Not to be confused with $5,000 Large)

    03/08/2018

    The 5th Generation of Mobile Wireless (5G) has been a hot topic of discussion for the past several years, and is likely about to be a hot economic topic and 5G trials and rollouts begin this year and next year. Most people are familiar with the upgrade from 3G to 4G, and appreciate the ability ..

    Read Full Article

    Did You Just Say EIRP? (Effective/Equivalent Isotropically Radiated Power)

    03/01/2018

    Effective, or equivalent, isotropically radiated power (EIRP) is a measurement of the optimum power that can be radiated from an antenna from a particular transmitter. Most often conveyed as either decibels (dB), or decibels over isotropic (dBi), EIRP is used to gauge the maximum possible radiation from an RF system, either for standards purposes or ..

    Read Full Article

    What is Antenna Polarization, and Why Does it Matter?

    02/22/2018

    Antenna polarization, much like polarization with light, and nothing to do with arctic weather, and everything to do with the transmission and reception of electromagnetic radiation based on its orientation. With light polarization, a film or glass will appear darker, and block, light which is polarized in a certain direction, while allowing correctly polarized light ..

    Read Full Article

    Massive-MIMO in a Nutshell

    02/15/2018

    It is no surprise that current and upcoming mobile wireless standards and methods are leveraging multiple technologies to increase the throughput to user equipment (UE) and the availability of high-speed data services. Some of the major challenges to overcome for high speed wireless data to be offered are limited spectrum availability, interference, and the sheer ..

    Read Full Article

    The Skinny on Skin Depth and Skin Effect

    02/08/2018

    The skin effect and skin depth is a rarely discussed topic, considering as it is an essential phenomenon to be aware of when working with any conductor, or semiconductor, at RF frequencies, or really anything other than DC. Essentially, the skin effect is the term to describe the way current is distributed in a conductor ..

    Read Full Article

    When and where are Flexible Waveguides Useful?

    02/01/2018

    Waveguide interconnect and assemblies are used in a wide variety of microwave and millimeter-wave applications. These applications include military, aerospace, Satcom, radar, microwave/millimeter-wave imaging, industrial heating/cooking, and more. In several of the applications and specific cases, a rigid waveguide assembly, or interconnect routing, must be done in a geometry which would require a waveguide structure ..

    Read Full Article

    What is a Magic-Tee, and Why Are They So Magical?

    01/25/2018

    A Magic-Tee is a 4-port waveguide structure similar to a rat-race coupler fabricated with striplines or microstrip waveguides. The Magic-Tee, or EH plane Tee, is able to perform an apparently “magical” function, which is to allow for energy going into the E and H plane ports to be divided between the two colinear ports while ..

    Read Full Article

    Why Are Frequency Band Designations So Confusing?

    01/18/2018

    A quick google search of “frequency bands” will often provide links to radio spectrum, cellular frequencies, spectrum bands, etc. If the searcher is so bold as to click on Wikipedia’s “Radio Spectrum” page, they will likely encounter tables with swaths of the electromagnetic spectrum designated by the International Telecommunication Union (ITU), IEEE, EU/NATO/US ECM, and ..

    Read Full Article
    Jump to of 31
    Live help