Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • Introduction to RF & Microwave Substrates & Base Materials

    09/05/2019

    The term “substrate” can be somewhat confusing the context of RF/Microwave devices, components, and applications. A substrate can generally be anything from the insulative material used to develop a semiconductor or film (thick-film or thin-film circuits or components), or the structural material of printed circuit boards (PCBs). These electrically insulating materials are the backbone of ..

    Read Full Article

    Roundup of RF Transistor Types, Semiconductors, and Configurations

    08/29/2019

    The growing number of RF, microwave, and millimeter-wave applications has led to a growth in the number of RF transistor types, semiconductors, and configurations being used today. As more devices use RF/wireless technology to communicate and sense, there will be an even greater diversity of RF transistor technologies. RF Amplifiers and RF Mixers are a ..

    Read Full Article

    What are Metamaterials and How Do They Relate to Antennas?

    08/22/2019

    Metamaterials are an increasingly researched topic, especially where it pertains to modern antenna structures. However, there is a lot of confusion of exactly what metamaterials are and how they are involved in the development of antennas. To put it simply, metamaterials are material and structure combinations that exhibit properties that are otherwise unknown to occur ..

    Read Full Article

    Note on GaN HEMT Amplifier Soft Compression

    08/15/2019

    Class III-V semiconductors, such as gallium arsenide (GaAs) and gallium nitride (GaN) have become commonplace solid state technologies for low noise amplifiers and high power amplifiers from frequencies ranging from several hundred megahertz to over 100 GHz. For high power applications, GaN high electron mobility devices (HEMTs) are supplanting GaAs metal-semiconductor field-effect transistor (MESFET) amplifiers, ..

    Read Full Article

    RF Transformer Tidbits

    08/08/2019

    RF Transformers are two, or more, port passive devices with a wide range of uses for many RF applications. One of the most common uses of an RF transformer is the Balun, which provides efficient coupling between unbalanced transmission circuits and balanced circuits. Other common uses are for impedance matching between circuits of different impedances. ..

    Read Full Article

    Voltage Controlled Oscillator Primer

    08/01/2019

    Voltage Controlled Oscillators (VCOs) are a key component to many tunable communications, radio, radar, sensing, and measurement systems. Essentially, a VCO is an oscillator that can be controlled by an input voltage, usually analog. Hence, adjusting the tuning voltage across its range also changes the VCOs output RF signal, proportionally. VCOs are used as key ..

    Read Full Article

    Coaxial and Waveguide Rotary Joints

    07/25/2019

    Rotary joints, unlike typical adapters, have the ability to rotate about the axis perpendicular to the wave propagation direction. While maintaining transmission properties, these joints can rotate freely 360 degrees. This type of joint is necessary for any application that has a rotating section, such as a rotary antenna (air surveillance), missile guidance system, and ..

    Read Full Article

    RF Test Equipment Series: Programmable Phase Shifters

    07/18/2019

    Controlling the phase of RF/microwave signals is an essential aspect of most modern communications, radar, and testing applications. Phase adjustments can be used to create a variety of effects, including combining, subtracting, and aligning signals, as well as part of phased-array antenna technology. Moreover, phase variations in a radar response can be used to distinguish important ..

    Read Full Article

    RF Test Equipment Series: RF/Microwave Power Sensors and Power Meters (Wattmeters)

    07/11/2019

    RF/microwave power sensors/meters, or wattmeters, are one of the simplest and most commonly used test instruments for diagnostics and repair of radio systems. These devices essentially extract a portion of the energy from an RF device or antenna, and using calibrated and traceable standards, present a power reading. RF Power sensors/meters are often used in ..

    Read Full Article

    RF Test Equipment Series: Software Defined Radios

    06/27/2019

    Software Defined Radios (SDRs) were once a poorly understood niche device, and have essentially overtaken the architecture of most radio devices, superseding hardware defined radios (HDRs). Most common types of modern test equipment have some form of SDR capability, meaning that at least some of their physical-layer functions are determined by software instead of hardware. ..

    Read Full Article
    Jump to of 31
    Live help