Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • 5G Update Series: Ultra-Reliable Low Latency Communication (URLLC)

    02/13/2020

    Ultra-reliable Low-latency Communications (URLLC) is a special use case of cellular communications that includes a set of features suited to low latency and ultra-high reliability applications. This includes mission critical applications, such as industrial automation, autonomous vehicles, smart grid, intelligent transportation/freight, and even augmented/virtual reality or remote medical or industrial procedures. It is commonly assumed ..

    Read Full Article

    Review of High Power Amplifier Applications: Class AB High Power Amplifiers

    02/06/2020

    A class AB amplifier is a highly used amplifier design for high power RF applications, as well as other applications that require high power gain with minimal signal distortion. The main feature benefit is that Class AB amplifiers are biased so that the output current flows for less than one full-cycle of the input waveform, ..

    Read Full Article

    5G Update Series: 5G Antenna Trends

    01/30/2020

    With the advent of the later 4G LTE releases (3GPP Release 13 and 14) and the latest 5G standard (3GPP Release 15), antennas for wireless telecommunications have begun to change substantially. Beyond the addition of sub-6 GHz frequencies for 5G, there are other technologies for enabling 5G use cases that are being developed that generate ..

    Read Full Article

    5G Update Series: Mission Critical Applications for 5G

    01/23/2020

    5G critical communications is one of the most sought after features of upcoming 5G networks. There are many industries, such as industrial robotics/factory automation, autonomous vehicles, traffic, public safety, fire, operations, emergency medical services, and even military/defense that all may benefit from enabling features and technology capabilities offered by mission critical 5G functions. One of ..

    Read Full Article

    5G Update Series: Massive Machine-type Communications IoT Update

    01/16/2020

    The goal of facilitating the growing data-centric behaviors of global society has led to new classifications of wireless communications. One of these new classifications defined in the 3GPP Release 13 is massive machine-type communications (mMTC). A new wireless technology, known as narrow-band Internet of things (NB-IoT) was created to enable communication between large numbers of ..

    Read Full Article

    RF Test Equipment Series: Load Pull Testing Primer

    01/09/2020

    Load Pull measurements is a class of non-50 Ohm measurements that is used during the design, model extraction, and performance testing of a variety of RF/Microwave devices. A main topic of discussion with load-pull testing is the evaluation of amplifier designs in a large signal sense. Load-pull testing essential consists of taking signal measurements from ..

    Read Full Article

    RF Test Equipment Series: PIM Analyzers

    12/19/2019

    Passive intermodulation distortion (PIM), is a prevalent issue with cellular networks and other wireless systems with relatively high broadcast power and dense channel plans. The results of PIM can be the desensitization of the receiver, dropped calls, and harmonic interference that can affect receivers for other frequency bands and services well outside of the carrier ..

    Read Full Article

    RF Test Equipment Series: Oscilloscopes

    12/12/2019

    An Oscilloscope is an essential piece of electrical test equipment, but has a somewhat limited use with RF circuits and systems compared to digital and analog circuits. In many cases an RF engineer will default to using a spectrum analyzer for frequency domain measurements and a network analyzer to measure component behavior. An oscilloscope is ..

    Read Full Article

    Pasternack 5G Discussion Series: Enhanced Mobile Broadband (EMBB)

    12/05/2019

    The planned technical expectations of 5G services are extreme in many ways. One of the most extreme use cases is the planned enhanced mobile broadband (eMBB) services, which are being designed to meet users growing demand for high speed data. The main features of eMBB are a massive increase in beak data rates, the ability ..

    Read Full Article

    RF Test Equipment Series: RF Anechoic Chambers

    11/21/2019

    RF anechoic chambers are used throughout the industry for prototyping testing and conformance testing. The purpose of an anechoic chamber is to provide both electromagnetic isolation from external sources as well as from internal RF radiation generators. Other types of testing that require complete RF isolation also depend on anechoic chambers, including radar cross section ..

    Read Full Article
    Jump to of 31
    Live help