Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • Early Eye on 3GPP Release 17

    04/30/2020

    Even though 3GPP Release 16 and Release 17 freeze dates have been moved back 3 months due to global events, there is still a good emerging picture of what 3GPP Release 17 specifications will tackle. Where the goal of Release 16 is to introduce standalone millimeter-wave 5G specifications, the focus of Release 17 is to ..

    Read Full Article

    What is a Variable Gain Amplifier (VGA)?

    04/23/2020

    A Voltage Variable, variable gain, or voltage controlled amplifier is a type of amplifier with a gain dependent on a control voltage input. These amplifiers are the backbone of amplitude modulation circuits. There are a wide range of types and styles of VCA’s that use various methods of controlling the gain. Some VCAs use voltage ..

    Read Full Article

    Rundown of Key Considerations of RF Surge Protectors for Telecommunications

    04/16/2020

    Coaxial RF surge protectors, or lightning arresters/surge suppressors, are important components that help protect sensitive radio and sensing electronics with external components or cabling from electromagnetic pulse (EMP) or other types of electrical surges. The basic function of these components is to short the transmission line to ground in the case of surge that exceeds ..

    Read Full Article

    RF ATE Systems Introduction

    04/09/2020

    Though there are many RF applications, especially those with operating frequencies in the upper microwave and millimeter-wave spectrum, that rely on hand assembly and testing, there are now an increasing number of RF applications that require automated test equipment (ATE) and systems. For instance, the sheer volume and repetitiveness of semiconductor wafers and chips is ..

    Read Full Article

    New Wireless Technologies 2020

    04/02/2020

    The following is a round-up of wireless technology trends predicted in 2020 and possible new wireless technologies we will see in the upcoming year. Major trends and drivers of wireless technology adoption New wireless standards specifically targeting new use cases outside of just cellular or wide-area-network communications. > Greater penetration of wireless technology across all ..

    Read Full Article

    Active Antennas versus Passive Antennas: The Difference between Active Antennas and Passive Antennas

    03/26/2020

    A passive antenna is a radiating element composed entirely of passive components. Typically, this means that a passive antenna system is one with at least a passive radiator (antenna element), passive impedance matching, passive balun, passive tuning (capacitive or inductive), and passive interconnect (commonly 50 Ohm or 75 Ohm impedance). A circulator or isolator may ..

    Read Full Article

    Temperature Conditioned Coaxial Cable Assemblies Explained

    03/12/2020

    There are many applications, some emerging, that require both phase and amplitude error to be minimized. These applications include synthetic aperture radar using antenna arrays, beamforming/MIMO antenna arrays for communications, actively electronically scanned array (AESA) radar, satellite communications, interference friend or foe (IFF) radar, and many other applications. Many of these applications must also place ..

    Read Full Article

    Preview of 3GPP Release 16 (5G Phase 2) – Standalone Millimeter-wave 5G

    03/05/2020

    Third generation partnership project (3GPP) is a standards body that is responsible for the major cellular telecommunication standards used to fuel cellular communication around the world. The latest standards release from 3GPP (Release 15) unleashed 5G new radio (NR) non-standalone (NSA) with enhanced mobile broadband (eMBB) features that add additional sub-6 GHz frequency bands and ..

    Read Full Article

    Basics of Waveguide Antennas

    02/27/2020

    A waveguide antenna is a type of antenna that channels RF energy from an air medium into a waveguide, or vice versa. Once the RF energy has been captured, it is either conducted through waveguide interconnect, or picked up by a coaxial interface to later be transmitted through a coaxial assembly. The reverse is also ..

    Read Full Article

    Introduction to Bi-phase Modulators

    02/20/2020

    A bi-phase modulator is a component of many complex IQ and quadrature modulator systems, and performs the task of two-state phase modulation (between 0 and 180 degrees) and is often paired with a continuously variable attenuator to provide both amplitude and phase modulation.. Bi-phase modulators can be used directly to produce binary phase shift keying ..

    Read Full Article
    Jump to of 31
    Live help