Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • RF Component & Device Test Series: Coaxial Cable Assembly Quality Testing

    04/01/2021

    Coaxial cable assemblies are at the heart of many conductive interconnect solutions from the module level to complete systems. Coaxial cable assemblies are used in a wide array of applications from low-cost connection of consumer equipment to extreme precision and reliability needed in aerospace and satellite communications. From R&D to defense, coaxial cable assemblies are ..

    Read Full Article

    Where Are We With 6G?

    03/25/2021

    5G is just on the cusp of deployment, with most mobile networks still operating on 4G-LTE technology. So, is it a bit early to be talking about 6G? Given that telecommunications service providers and technology developers have somewhat settled on a new generation of cellular wireless technology every 10 years, this means that 6G is ..

    Read Full Article

    Updates on RF Silicon Technology

    03/18/2021

    Though Gallium Nitride (GaN) has been making headlines for the past several years as an emerging RF technology, RF semiconductors developed with silicon, namely RF silicon-on-insulator (RF-SOI), has also been advancing as a semiconductor of choice for the exploding RF hardware markets.  Where GaN is a still relatively expensive and small wafer technology, RF-SOI is ..

    Read Full Article

    RF/Microwave Test Equipment Useful for EMC Precompliance Testing

    03/11/2021

    Virtually every country around the world has some type of electromagnetic compliance (EMC) policy in place to prevent hazardous emissions, susceptible electronics in the marketplace, and to avoid an overabundance of interference. Given the complex nature of EMC, most compliance codes are very strict and the cost of failure is that a product cannot be ..

    Read Full Article

    Overview of High Power RF Attenuators

    03/04/2021

    RF Attenuators come in a wide variety of packages, technologies, and performance ranges. Some RF attenuator technology is compact enough to fit on an IC, while some units are large enough to require internal and/or external thermal management systems. The size and significance of the thermal management of an RF attenuator depends on the attenuator ..

    Read Full Article

    Signal Chain Discussion Series: Impedance Matching

    02/25/2021

    An RF Signal Chain is generally composed of a series of RF devices and components, each with their own unique behavior. In every case, however, each component and device within the signal chain presents an impedance at their input ports and output ports. Moreover, the interconnect between devices and components within a signal chain also ..

    Read Full Article

    5G Updates

    02/18/2021

    Though 2020 has posed many challenges for economies and consumers around the world, 5G deployments and developments continued. Many industries are putting a substantial amount of their stock in the economic potential that 5G services should provide. Given the remote working/work-from-home and remote schooling situations many continue to find themselves in, there may be an ..

    Read Full Article

    Primer On Millimeter-wave Test Interconnect Challenges Including 5G

    02/11/2021

    The rise of emerging millimeter-wave applications has begun to change the landscape of millimeter-wave device and system testing. In previous years, millimeter-wave applications were the purview of scientific research, military/defense, and satellite communications. These applications are typically comfortable with low-volume production, high single-unit costs, long lead times, custom solutions, and labor-intensive testing/quality/verification methods. Unlike previous ..

    Read Full Article

    Signal Chain Discussion Series: Filters

    02/04/2021

    RF filters are passive or active components commonly used in the signal chain of virtually all radio and RF sensing technologies. The main purpose of a filter is to significantly attenuate unwanted portions of the spectrum, or specific frequencies, while only minimally impacting the operating frequencies. RF filters are typically constructed of various resonator technologies ..

    Read Full Article

    Overview of Ferrite-based RF Technology

    01/28/2021

    Ferrites are high electrical resistance, magnetic, and ceramic materials constructed from a mix of metallic oxides, often including Iron (Fe), Zinc (Zn), Manganese (Mn), Nickel (Ni), Cobalt (Co), Barium (Ba), and Strontium (Sr). These metallic oxides exhibit magnetic behavior that allows for their use in RF circuits as inductors, transformers/baluns, isolators, circulators, phase shifters, chokes, ..

    Read Full Article
    Jump to of 31
    Live help