Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • Advantages of the Double Ridge Waveguide Design

    07/01/2021

    Waveguides come in many varieties. The most common “shapes” for waveguide cross sections are rectangular and circular/oval. Waveguide can carry electromagnetic energy in several modes, though they are typically specified for a primary mode that presents the most desirable characteristics for loss and bandwidth. This mode is generally the transverse electric (TE) mode, where the ..

    Read Full Article

    RF Component & Device Test Series: RF Filter Testing

    06/17/2021

    RF Frequency filters, or just filters, are components/devices that modify a signal’s amplitude and phase angle based on frequency. Filters are either passive or use active tuning electronics. Filters are designed with a predetermined frequency dependent transmission response and are predominately used to attenuate portions of the spectrum where undesirable signal components, interference, or noise ..

    Read Full Article

    RF Component & Device Test Series: RF Low Noise Amplifier Testing

    06/03/2021

    Low noise amplifiers (LNAs) are a critical component for telecommunication and sensing systems, as the weak receive signals often need to be at a higher signal level for optimal demodulation, digitization, driving another circuit, or for measurements to be made. LNAs are also used throughout signal chains to add gain to low power signals when ..

    Read Full Article

    RF Component & Device Test Series: How Are Active RF Devices Tested

    05/20/2021

    RF devices are active elements in the RF signal chain and are used in almost all RF systems with exception of purely passive systems. Active RF devices are distinguished from passive RF devices in that electrical power or electrical control signals are used to energize the device and change its performance. In many cases, active ..

    Read Full Article

    RF Component & Device Test Series: How Are RF Passive Devices Tested

    05/13/2021

    RF passive components are used in virtually every RF assembly and system for communications, sensing, and test and measurement applications. Hence, testing RF passives is critical to all applications. RF passives testing may be for characterization, quality control/verification, or maintenance/troubleshooting depending on the use case of the RF passive and if it is under development, ..

    Read Full Article

    Microwave Measurement Methods of Dielectrics

    05/06/2021

    Conductors, semiconductors, and insulators are the main building blocks of virtually all RF/microwave electronics. Insulators have dielectric properties that impact the electric fields that pass through them. In order to design an RF component or device, detailed knowledge of the dielectric properties of the insulators used in the construction of the component/device is essential. The ..

    Read Full Article

    Waveguide Amplifier Introduction & Applications

    04/29/2021

    Waveguide amplifiers are amplifiers specifically designed to be housed within a waveguide assembly. This provides some intrinsic advantages and trade-offs compared with coaxial connectorized amplifier assemblies or pallet amplifiers. Given that waveguide amplifiers are designed to directly mate with a given waveguide size and type, they are innately banded, as the waveguide has a limited ..

    Read Full Article

    RF Applications Series: Buried Object Detection Using Ground Penetrating Radar

    04/22/2021

    Ground penetrating radar (GPR) is a technology that uses pulses of electromagnetic energy sent into the ground to create reflections from the ground compositions and objects within the ground. These reflections can then be analyzed by software and turned into a plot or map projection so that objects within the ground can be identified or ..

    Read Full Article

    RF Component & Device Test Series: Coaxial Cable Assembly Performance Testing Part 2

    04/15/2021

    In part 1 of this series we delved into several of the commonly specified electrical performance characteristics for coaxial cable assemblies. This post wraps up the most common parameters: •  Capacitance •  Group Delay •  Velocity of Propagation •  RF Shielding/Leakage •  Maximum Input Power (Power Handling) •  Maximum Voltage/Breakdown Voltage •  Phase Stability (during ..

    Read Full Article

    RF Component & Device Test Series: Coaxial Cable Assembly Performance Testing Part 1

    04/08/2021

    In the previous post we explored quality testing of coaxial cable assemblies. In this post, we are exploring the electrical performance testing of coaxial cable assemblies. The following is a list of the most common electrical performance parameters given for coaxial cable assemblies. Key Coaxial Assembly Performance Tests • Frequency Range (Cutoff Frequency) • Insertion ..

    Read Full Article
    Jump to of 31
    Live help