Live Help
x Start Chat

Armored vs. Unarmored: When to Use Ruggedized Test Cables in the Field

  • Categories

  • Archive

  • RF and microwave testing has expanded far beyond controlled laboratory environments. Vector network analyzers and other RF test equipment are now routinely deployed on factory floors, production lines and outdoor field sites where environmental stress, repeated handling and physical hazards are unavoidable.

    As testing moves closer to real-world operating conditions, cable durability becomes just as critical as electrical performance. A damaged or unstable test cable can introduce measurement errors, force recalibration and cause costly downtime. Selecting between armored and unarmored test cables is no longer a cosmetic choice. It’s a critical selection that directly impacts accuracy, repeatability and test throughput.

    Key Takeaways

    • Field and production testing place greater mechanical stress on test cables than lab environments
    • Armored test cables prioritize durability and lifecycle stability
    • Unarmored test cables offer maximum flexibility for controlled setups
    • Choosing the right cable reduces measurement drift, downtime and rework

    Explore Test & Measurement Solutions

    When VNA Testing Leaves the Lab

    Traditional RF testing assumed static cable routing, limited movement and controlled handling. Today, VNA measurements often occur in environments where cables are flexed repeatedly, routed around equipment or exposed to vibration, abrasion and operator handling.

    In these conditions, cable failures rarely appear as total loss. More often, they show up as subtle phase or amplitude instability that degrades measurement confidence. The hidden cost of these failures includes repeated calibrations, inconsistent test results and delayed production schedules.

    Ruggedized test cable design helps mitigate these risks by addressing both electrical stability and mechanical resilience.

    Characteristics of Armored Test Cables

    Armored test cables are designed for environments where mechanical protection and long-term durability are priorities.

    Key construction features include:

    • Stainless steel or braided armor that protects against crushing, abrasion and torque
    • Reinforced strain relief to reduce connector stress during flexure
    • Jackets designed to withstand UV exposure, vibration and repeated handling

    From a durability standpoint, armored cables are built to survive high-cycle flexing, frequent connect and disconnect cycles and harsh environments without compromising measurement stability.

    Characteristics of Unarmored Test Cables

    Unarmored test cables are optimized for flexibility and ease of routing in controlled environments.

    Common characteristics include:

    • Lightweight construction with minimal outer protection
    • Smaller bend radius for tight test setups
    • High phase and amplitude stability when movement is limited

    These cables are well suited for laboratory benches, calibration setups and applications where cables remain mostly static and protected from physical stress.

    Armored vs. Unarmored: Key Performance Tradeoffs

    Choosing between armored and unarmored test cables involves balancing electrical performance with mechanical requirements.

    Electrical Performance Considerations
    Both cable types can deliver excellent VSWR, insertion loss and phase stability when properly designed. However, real-world performance depends on how much the cable moves after calibration. Armored cables often maintain phase stability more consistently in dynamic environments due to their mechanical reinforcement.

    Mechanical Durability and Lifecycle
    Armored cables offer significantly longer service life in environments with frequent flexing, operator handling or exposure to physical hazards. Unarmored cables may degrade faster under the same conditions, even if electrical specifications appear similar on paper.

    Key Considerations for Choosing the Right Cable

    Selecting the right test cable starts with understanding how and where it will be used.

    Assessing the Environment

    • Controlled lab versus factory floor or outdoor site
    • Exposure to vibration, abrasion or crushing forces
    • Frequency of cable movement after calibration

    Evaluating the Type of Equipment and Tests

    • VNA testing versus handheld analyzers
    • Static measurements versus repeated connect and disconnect cycles
    • Sensitivity to phase and amplitude variation

    Considering Cable Length and Connectivity Needs

    • Longer cables experience greater mechanical stress
    • Connector types and mating cycle requirements
    • Routing complexity around equipment

    When Armored Test Cables Are the Better Choice

    Armored test cables are typically the better option when testing extends beyond controlled lab conditions. They are well suited for production environments, in-field measurements, high-cycle test setups and applications where cables are frequently repositioned.

    In these scenarios, the added mechanical protection helps maintain measurement integrity, reduce recalibration frequency and extend cable service life.

    Choosing the Right Test Cable for Your Environment

    The most effective cable selection balances flexibility, durability and RF performance.

    Key questions to evaluate include:

    • Is the test environment static or dynamic
    • Will the cable be moved after calibration
    • Is durability or maximum flexibility the higher priority
    • Skill level / control of the users (engineers will usually treat it better than operations)

    Aligning cable selection with long-term throughput goals helps ensure reliable measurements, consistent results and lower total cost of ownership.

    Explore Pasternack’s trusted and tested lineup of RF breakout test cable assemblies and connectors for testing applications.

    https://www.pasternack.com/rf-test-leads-and-breakouts-category.aspx

    Matching Cable Design to Real-World Testing Demands

    As RF testing continues to move closer to real-world environments, test cables must perform reliably under mechanical stress as well as electrical scrutiny. Armored and unarmored test cables each serve a purpose, but choosing the wrong type can lead to measurement drift, downtime and reduced confidence in results.

    By matching cable design to the realities of lab, production or field testing, engineers can maintain accuracy, improve efficiency and ensure test setups remain reliable over time.

    Frequently Asked Questions

    What is the main difference between armored and unarmored test cables?
    Armored test cables include mechanical protection to resist crushing, abrasion and torque, while unarmored cables prioritize flexibility and lightweight handling.

    Are armored test cables less flexible than unarmored cables?

    Yes. Armored cables are generally less flexible, but they offer greater durability and phase stability in dynamic or harsh environments.

    When are armored test cables worth the investment?
    Armored test cables are worth the investment in environments where cables are frequently moved, flexed or exposed to mechanical stress. The added protective layer helps prevent damage to the cable assembly, extend service life and maintain measurement stability over time. In controlled laboratory settings where cables remain mostly static and protected from physical stress, unarmored cables are often sufficient and can offer a more cost-effective option.

    Do armored cables affect VNA measurement accuracy?
    When properly designed, armored cables maintain excellent electrical performance and often provide more consistent results in environments with frequent movement.

    How does cable durability impact long-term testing costs?
    More durable cables reduce failures, recalibration time and downtime, lowering the total cost of ownership in production and field-testing environments.

    Live help