Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • Portable VNA Calibration: Essential Kits for Field Service Technicians

    03/25/2026

    Portable vector network analyzers (VNAs) have become indispensable tools for RF and microwave measurements outside the laboratory. Field service technicians rely on portable VNAs to validate antenna systems, troubleshoot cables and verify RF performance in real-world environments where conditions are far less controlled than a lab bench. Accurate measurements in these environments depend on proper calibration. Without reliable calibration ..

    Read Full Article

    Phase Matching: Ensuring Synchronization in Multi-Channel Radar Systems

    Modern radar systems rely on precise timing and signal alignment across multiple channels to operate correctly. Whether used for surveillance, navigation or defense applications, multi-channel radar systems depend on accurate phase synchronization to form beams, resolve targets and maintain system integrity. Even small phase mismatches between channels can degrade performance, reduce accuracy and complicate system validation. As radar architectures become more complex and testing moves from controlled labs into ..

    Read Full Article

    Interpreting VSWR and Return Loss Data from Your Cable Test Reports

    Voltage Standing Wave Ratio (VSWR) and return loss are two of the most common metrics included in RF cable test reports, yet they are also among the most misunderstood. While both measurements describe signal reflections, correctly interpreting the data is critical for evaluating cable quality, diagnosing performance issues and ensuring reliable RF system operation. For engineers working ..

    Read Full Article

    How Often Should You Calibrate Your RF Test Cables? A Maintenance Schedule

    Calibration is fundamental to accurate RF and microwave measurements, yet test cables are often treated as passive accessories rather than critical measurement components. In reality, RF test cables play an active role in signal integrity and measurement accuracy, especially as frequencies increase and test environments become more demanding. Unlike instruments, cables are subject to mechanical stress, flexing and environmental exposure. Assuming calibration is ..

    Read Full Article

    Reducing Test Setup Time: The Role of Quick-Connect Adapters and Presets

    RF testing environments are under increasing pressure to deliver fast, repeatable results without compromising accuracy. Industries such as 5G, aerospace and defense, and electronics manufacturing demand high-throughput testing while maintaining tight control over measurement quality. Traditional VNA setups, originally designed for lab-based precision testing, often struggle to scale on production floors. Manual connections, repeated recalibration and inconsistent setup practices introduce delays, variability and ..

    Read Full Article

    Armored vs. Unarmored: When to Use Ruggedized Test Cables in the Field

    03/24/2026

    RF and microwave testing has expanded far beyond controlled laboratory environments. Vector network analyzers and other RF test equipment are now routinely deployed on factory floors, production lines and outdoor field sites where environmental stress, repeated handling and physical hazards are unavoidable. As testing moves closer to real-world operating conditions, cable durability becomes just as critical as electrical performance. A damaged ..

    Read Full Article

    Weatherproofing Your Test Gear: IP Ratings for RF Interconnects

    RF testing no longer happens exclusively in clean, climate-controlled laboratories. VNAs and associated test gear are increasingly deployed on production floors, outdoor sites and field installations where environmental exposure is unavoidable. Dust, moisture, temperature variation and mechanical vibration all pose risks to RF measurement accuracy. Without proper environmental protection, these factors introduce instability, accelerate wear ..

    Read Full Article

    The Risks of “Drift”: How Temperature Changes Affect Calibration Accuracy

    Calibration drift is one of the most difficult accuracy problems to detect in RF and microwave testing. Unlike obvious failures, drift develops gradually, quietly shifting measurements away from calibrated reference points without triggering alarms or hard errors. Temperature change is one of the most common and underestimated causes of drift. Whether in a climate-controlled lab, ..

    Read Full Article

    The Hidden Cost of “Cheap” VNA Cables in High-Volume Production Lines

    Vector network analyzers play a central role in high-volume RF and microwave manufacturing, verifying performance, catching defects and protecting product quality before shipment. Yet in many production environments, test cables are treated as consumables rather than critical measurement assets. This mindset often leads to the use of low-cost VNA cables that appear acceptable on a specification sheet but fail to hold ..

    Read Full Article

    Testing 5G Infrastructure: Essential Cables for 40 GHz Outdoor Measurements

    The rollout of 5G infrastructure has transformed how wireless networks are designed, deployed and tested. Higher data rates, lower latency and support for massive device connectivity place new demands on RF measurement systems, particularly as networks extend into higher frequency ranges. Testing 5G infrastructure at 40 GHz introduces challenges that go beyond traditional sub-6 GHz measurements. Outdoor environments, long ..

    Read Full Article
    Jump to of 3
    Live help