Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • Harnessing the Potential of the 110 MHz Frequency with Broadband Amplifiers

    02/27/2024

    Whether used in communication networks, broadcasting systems, or advanced testing environments, the 110 MHz frequency requires precision tools to amplify signals and minimize interference. In communication networks, broadcasting systems, or advanced testing environments, this frequency requires precision tools to amplify signals and minimize interference. Tools like 110 MHz frequency broadband amplifiers ensure seamless signal transmission ..

    Read Full Article

    Demystifying Low Loss Coaxial Cable Terms

    02/22/2024

    When looking into coaxial cable for a variety of applications, from commercial wireless to audio/visual broadcast, it is not uncommon to come across coaxial cable types labeled as LMR-, CFD-, OFC-, etc. at several different indicators, such as 195, 200, 240, 400, or 600. An example of this is Low Loss Flexible LMR-400 Plenum Rated ..

    Read Full Article

    How to Calculate Frequency from Wavelength

    02/15/2024

    The concept of calculating frequency from wavelength is fundamental in the study of waves, including electromagnetic waves like light and radio. Understanding how these two properties relate, and how to calculate frequency from wavelength, can be useful in fields like telecommunications, physics, and engineering. Whether you’re working with sound waves, microwaves, or visible light, being ..

    Read Full Article
    Jump to of 1
    Live help