Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • What Is A 2.4 GHz Antenna?

    01/25/2024

    There is a plethora of wireless communications antennas labeled as a 2.4 GHz antenna, this does not mean that these antennas only operate at exactly 2.4 GHz. It implies that they cover some area of the 2.4 GHz ISM band, which extends from 2.4 GHz to 2.5 GHz. In most cases, for the 2.4 GHz ..

    Read Full Article

    What Does RF Stand For?

    01/11/2024

    Simply, RF stands for Radio Frequency. This generally refers to all of the electromagnetic spectrum that is used for radio systems and wireless communication. However, RF can also mean a variety of different things depending on the context of use. On some occasions when discussing spectrum, RF refers to the frequency range below microwaves, which ..

    Read Full Article

    The Benefits and Uses of the Right Angle 3.5mm Adapter

    01/03/2024

    For engineers, testers, and hobbyists working with radio frequency (RF) equipment, the right angle 3.5mm adapter stands out as a particularly valuable tool. Often used in systems requiring compact arrangements or challenging angles, right angle coax adapters ensure seamless connectivity without compromising signal integrity. Not only does a right angle 3.5mm adapter save space, but ..

    Read Full Article
    Jump to of 1
    Live help