Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • Wi-Fi Next Generation (Wi-Fi 7) Updates

    11/23/2023

    The next generation of Wi-Fi, IEEE 802.11be, or Wi-Fi 7 standard, is slated to be officially released in early 2024. However, there are already a host of devices on the market that are touting Wi-Fi 7 capabilities, as early drafts of the standard have been regularly released as the amendment has been developed. This means ..

    Read Full Article

    What is a D-Sub Connector/Contact?

    11/09/2023

    D-Sub, or D-Subminiature, connectors are used in a variety of applications from military/defense to commercial technology and computer/networking technology. D-Sub connectors can be used for power, analog, RF, or digital signal transmission, and are often readily repaired/replaced/installed in the field. This connector style is extremely versatile and can be found anywhere from temperature-controlled data centers ..

    Read Full Article

    Why 2.4mm Connectors Are the Backbone of High-Frequency, Eco-Compliant RF Systems

    11/05/2023

    In the world of RF and microwave engineering, 2.4mm connectors are indispensable, particularly in high-frequency and precision applications. Designed with a focus on handling high-frequency signal applications, these RF connectors are key to industries that require low-loss signal integrity and robust connectivity, such as telecommunications, aerospace, and advanced research labs. Because they also satisfy stringent ..

    Read Full Article
    Jump to of 1
    Live help