Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • Signal Chain Discussion Series: Local Oscillators

    12/17/2020

    A local oscillator (LO) is an electronic oscillator that generates a very narrow bandwidth signal, or tone, with high purity and stability for use in frequency conversion circuits and timing. As the performance of frequency conversion circuits and timing systems are often dependent on the LO performance, the quality of the oscillator and LO electronic ..

    Read Full Article

    Signal Chain Discussion Series: Difference Between IF & RF

    12/10/2020

    In many cases in RF/Microwave electronics it is advantageous to generate, modulate, receive, and demodulate communication and sensing signals at frequencies lower than the RF transmission/reception carrier frequency. The frequency difference between the modulation/demodulation (baseband) signals and the RF signals may be so vast, that multiple frequency conversion stages may be required. In these instances, ..

    Read Full Article

    Signal Chain Discussion Series: Circulators & Isolators Versus Switches As Duplexers

    12/03/2020

    Circulators/isolators and switches are both commonly used in the RF front-end of communication and radar systems. The purpose of circulators/isolators and switches in RF front-ends is to enable the use of transmission and reception from the same antenna, duplexing. For instance, in a transmit/receive module (TRM) for an active antenna system (AAS) (phased array antenna), ..

    Read Full Article
    Jump to of 1
    Live help