Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • Distributed Antenna System (DAS) Basics

    03/29/2018

    There are many cases, especially within buildings, tunnels, large public venues, stadiums, and etc. where the signals from a cell tower does not provide sufficient coverage, or the density of users is just too great for a typical cellular approach. In these circumstances DAS installation can be employed to enhance the coverage in these areas, ..

    Read Full Article

    Small Cells are Certainly Making a Large Impact

    03/15/2018

    Small Cells are essentially a mobile wireless installation that is smaller in scope and size than a traditional macro base station. So, why are Small Cells, which provide less coverage and necessarily are composed of equipment that may not have the full capability of macro-cells, on the rise? An important note is that the term ..

    Read Full Article

    The 5th Generation of Mobile Wireless (Not to be confused with $5,000 Large)

    03/08/2018

    The 5th Generation of Mobile Wireless (5G) has been a hot topic of discussion for the past several years, and is likely about to be a hot economic topic and 5G trials and rollouts begin this year and next year. Most people are familiar with the upgrade from 3G to 4G, and appreciate the ability ..

    Read Full Article

    Did You Just Say EIRP? (Effective/Equivalent Isotropically Radiated Power)

    03/01/2018

    Effective, or equivalent, isotropically radiated power (EIRP) is a measurement of the optimum power that can be radiated from an antenna from a particular transmitter. Most often conveyed as either decibels (dB), or decibels over isotropic (dBi), EIRP is used to gauge the maximum possible radiation from an RF system, either for standards purposes or ..

    Read Full Article
    Jump to of 1
    Live help