Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • When DAS Meets PIM: On the Challenges of Accounting for PIM with Distributed Antenna Installations (Part 2)

    04/11/2019

    In last week’s post, we covered foundational details regarding PIM in modern wide-band and multi-carrier communication systems, with a note on upcoming 5G NR sub-6 GHz frequencies being added to the mix. This week’s blog expands upon that discussion and provides more details of PIM considerations specific to DAS. With DAS, another large PIM concern ..

    Read Full Article

    When DAS Meets PIM: On the Challenges of Accounting for PIM with Distributed Antenna Installations (Part 1)

    04/04/2019

    Passive intermodulation distortion is the result of discontinuities, metal-to-metal contact, and material properties that lead to nonlinear characteristics of typically linear passive transmission lines and components. PIM can be induced in a variety of RF components, such as connectors, adapters, cable, combiners, splitters, couplers, tappers, attenuators, terminators, antennas, and cable-to-board interconnect. PIM is generated when ..

    Read Full Article

    Coaxial Cable Assemblies Aren’t the Only Low PIM Devices (Tappers, Splitters, Couplers, Loads, Adapters, and Antennas) Part 2

    03/28/2019

    Last week’s post covered why low PIM components, other than coaxial cables and assemblies, can be important to consider for low PIM applications. This blog focuses on low PIM Directional Couplers, Loads, Attenuators, Adapters, and Antennas, and provides brief descriptions of their use cases and value. Low PIM Directional Couplers Unlike tappers, splitters, and dividers, ..

    Read Full Article

    Coaxial Cable Assemblies Aren’t the Only Low PIM Devices (Tappers, Splitters, Couplers, Loads, Adapters, and Antennas) Part 1

    03/21/2019

    Passive intermodulation distortion (PIM) is phenomenon that degrades communication system performance in virtually all DAS and cellular installations. The severity of PIM, and the measures necessary to mitigate PIM depend on the system design, materials, environment, transmit power, and the systems sensitivity to PIM. Single frequency and narrow band communications technologies tend to be less ..

    Read Full Article

    The Making of Low PIM Coaxial Cable Assemblies

    03/14/2019

    With the growing number of distributed antenna system (DAS) and small cell installations, low passive-intermodulation distortion (PIM) interconnect and components have gained popularity. Modern complex multi-carrier communication systems, such as DAS and small cells, are now incredibly wide-band and support a plethora of wireless standards, such as WiFi, cellular, military, government, public safety, and emergency ..

    Read Full Article

    Low PIM Formable Cable Jumpers Introduced

    07/21/2014

    Low PIM Cable Assemblies Utilizing a Hand Formable Semi-Rigid Coax Debuted Pasternack’s low PIM hand formable cable jumpers are made using a tin-filled braid that produces a hand-formable, solid outer conductor wall, making them perfect for installation into tight places. These low passive intermodulation (PIM) cable assemblies are available with two different coax diameters sizes ..

    Read Full Article
    Jump to of 1
    Live help