Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • All About D-Sub Connectors

    04/04/2024

    D- Subminiature connectors, or D-Sub connectors, are a compact and versatile connector platform that can support power, analog, RF, or digital signal transmission. Depending on the type of D-Sub Connectors used, a D-Sub connector could support connections from every domain, which makes these an extremely common connector interface for a wide range of applications. These ..

    Read Full Article

    Difference Among Coplanar Waveguide Microstrip, Stripline, and Other Planar Transmission Lines

    02/23/2023

    Planar transmission lines are used to carry a variety of analog, RF, and digital signals on insulative, planar substrates from kilohertz to hundreds of gigahertz frequencies. Planar transmission lines are constructed of one or more layers of conductive traces, possibly with adjacent conductive structures, with dielectric layers providing insolation between the conductive structures. Planar transmission ..

    Read Full Article

    Power Added Efficiency (PAE) Calculator Explained

    12/01/2022

    RF power amplifiers typically have an input, output, and power supply rails. These rails can be either positive, negative, or dual positive and negative voltages. The input, output, and power supply rails all have recommended operating ranges of power, voltage, and current. This range is specified to nominal operation in what the manufacturer was able, ..

    Read Full Article

    Pasternack’s 50th Anniversary! An Interview with the Man who Started it all

    11/14/2022

    Pasternack has a milestone anniversary this year! Fifty years later, Pasternack products are as relevant and renowned as ever, and there’s no slowing down. To celebrate this momentous occasion, we recently had the opportunity take a trip down memory lane and learn the history of the brand from Murray Pasternack, the founder of Pasternack. Read ..

    Read Full Article

    VSWR, Return Loss, Insertion/Transmission loss vs. Transmission Power

    09/22/2022

    In an ideal RF system, all of the energy from the RF source is transferred to the load. An example of this would be a transmitter delivering a signal to an antenna with the interconnect between the two signal chain components operating at 100% efficiency. Clearly, this isn’t the case, and factors like impedance mismatch ..

    Read Full Article

    Dielectrics at High Frequencies

    11/18/2021

    Dielectrics are one of the three main categories of electrical materials, the other two being conductors and semiconductors. Common dielectrics used in electronic systems are ceramics, glasses, gemstones, and polymers. Dielectrics, or insulators, are described as being very poor electrical conductors, and unlike conductors, allow for electrical fields to pass through them. However, the electric fields ..

    Read Full Article

    Microwave Measurement Methods of Dielectrics

    05/06/2021

    Conductors, semiconductors, and insulators are the main building blocks of virtually all RF/microwave electronics. Insulators have dielectric properties that impact the electric fields that pass through them. In order to design an RF component or device, detailed knowledge of the dielectric properties of the insulators used in the construction of the component/device is essential. The ..

    Read Full Article

    Updates on RF Silicon Technology

    03/18/2021

    Though Gallium Nitride (GaN) has been making headlines for the past several years as an emerging RF technology, RF semiconductors developed with silicon, namely RF silicon-on-insulator (RF-SOI), has also been advancing as a semiconductor of choice for the exploding RF hardware markets.  Where GaN is a still relatively expensive and small wafer technology, RF-SOI is ..

    Read Full Article

    Overview of Ferrite-based RF Technology

    01/28/2021

    Ferrites are high electrical resistance, magnetic, and ceramic materials constructed from a mix of metallic oxides, often including Iron (Fe), Zinc (Zn), Manganese (Mn), Nickel (Ni), Cobalt (Co), Barium (Ba), and Strontium (Sr). These metallic oxides exhibit magnetic behavior that allows for their use in RF circuits as inductors, transformers/baluns, isolators, circulators, phase shifters, chokes, ..

    Read Full Article

    Signal Chain Discussion Series: Difference Between IF & RF

    12/10/2020

    In many cases in RF/Microwave electronics it is advantageous to generate, modulate, receive, and demodulate communication and sensing signals at frequencies lower than the RF transmission/reception carrier frequency. The frequency difference between the modulation/demodulation (baseband) signals and the RF signals may be so vast, that multiple frequency conversion stages may be required. In these instances, ..

    Read Full Article
    Jump to of 6
    Live help