Live Help
x Start Chat

Pasternack Blog

  • Categories

  • Archive

  • New Low Profile, Right Angle Test Cable Line Up to 27 GHz

    05/24/2016

    New SMA, Type N and TNC Test Cable Boast 1.25:1 Typical VSWR and 69.5% Phase Velocity We just launched a new family of right angle test cable with low profile design. These 16 unique test cable assemblies cover a frequency range from DC to 27 GHz for the SMA versions and DC to 18 GHz ..

    Read Full Article

    60 GHz Development System Kit Offers a Quick Out-of-the-Box Experience for Evaluating High Bandwidth Data Rates in the Unlicensed ISM Frequency Spectrum

    05/20/2016

    60 GHz Product Development System and Experimentation Kit for High Bandwidth Modulation Covering 57 to 64 GHz Made Easy The new 60 GHz development system kit, now with even lower phase noise,  offers designers the ability to perform millimeter wave product development and conduct RF experimentation. The developer kit for 60 GHz provides single and ..

    Read Full Article

    IMS 2016 IEEE MTT-S San Francisco, CA Pasternack Drone Contest

    05/17/2016

    We will be exhibiting at the IMS 2016 conference, convention and exposition which is now called the International Microwave Symposium 2016, formerly called MTT-S or the Microwave Theory and Techniques Society trade show, being held in San Francisco, CA for 2016. The IMS 2016 General Chair says “IMS2016, organized by the IEEE Microwave Theory and ..

    Read Full Article

    IEEE / MTT-S / International Microwave Symposium / IMS 2016

    05/09/2016

      Again this year we will be exhibiting at the IEEE conference, convention and exposition called the International Microwave Symposium / IMS, formerly called MTT-S or the Microwave Theory and Techniques Society trade show, which is held in San Francisco, CA for IMS 2016. According to the IEEE conference website previously, “the IEEE MTTS International ..

    Read Full Article

    PIN Diode Switch RF Product Line Now Largest Same Day Ship Selection

    04/28/2016

    Pasternack PIN Diode Switch Expanded to the Largest In-Stock, Same-Day Ship Inventory We greatly expanded our PIN diode switch products over the past several months to become THE source for your needs. Pasternack can now claim the largest selection of connectorized PIN diode switches in-stock for same day shipping. Our portfolio of in-stock solid state ..

    Read Full Article

    New Network Analyzer VNA Cable Series for 50 GHz and 67 GHz Millimeter Wave Testing

    03/21/2016

    50 GHz and 67 GHz Millimeter Wave VNA Cables We debuted a new line of flexible, precision millimeter wave VNA cables rated to 50 and 67 GHz …depending on the series of course. Designed for use as cables for VNA test port extension, these highly durable and flexible VNA test cables are able to withstand ..

    Read Full Article

    The Cable Creator™ for Custom Coaxial RF Cable Assemblies Updated

    02/15/2016

    We just released an improved version of our popular online standard and custom coaxial RF cable assemblies tool called The Cable Creator™. This new custom RF coaxial cable assembly tool iteration allows the user to not only design and customize special radio frequency cable configurations online in a few clicks, but also purchase their designs ..

    Read Full Article

    Rackmount Variable Gain RF Amplifier with Performance from 100 MHz to 18 GHz

    01/18/2016

    We just launched a brand new rackmount variable gain RF amplifier with performance from 100 MHz to 18 GHz. This Pasternack 19-inch rack mounted RF amplifier is designed for lab use and various test and measurement applications. Normally this type of RF rack mount amplifier requires long lead-times for delivery often exceeding several months; however, ..

    Read Full Article

    Flexible Waveguide Product Line expanded

    12/27/2015

    We expanded our flexible waveguides product portfolio with the addition of new products that operate up to 40 GHz over nine frequency bands. This offering consists of 36 unique models of flexible waveguide twists ranging in size from WR-137 (as low as 5.85 GHz) to WR-28 (up to 40 GHz). These Pasternack twistable flexible waveguides, also ..

    Read Full Article

    RF Engineering and Technical Support Education Courses Offered to Pasternack Customers Through Besser Associates

    11/05/2015

    We have partnered with Besser Associates to offer customers a seamless portal for accessing continuing radio frequency education courses in the fields of RF, microwave and millimeter wave technologies. RF engineering and technical support personnel needing continued education in radio frequency courses both online and school classroom environment have Besser Associates as an option through ..

    Read Full Article
    Jump to of 5
    Live help